![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This defines the DSA sensor configuration parameter structure configuring the sensor settings by a subscriber task. More...
#include <isf_dsa_adapter.h>

Data Fields | |
| isf_fifo_t * | pSampleBufferInfo |
| uint32 | nSamplePeriod |
| isf_SensorDataTypes_t | resultType |
| isf_dsa_result_types_t | resultFormat |
This defines the DSA sensor configuration parameter structure configuring the sensor settings by a subscriber task.
Definition at line 79 of file isf_dsa_adapter.h.
| uint32 nSamplePeriod |
Sample period in microseconds.
Definition at line 82 of file isf_dsa_adapter.h.
Referenced by configure_sensor(), fsl_fusion_virt_3D_orient_Configure(), fsl_fusion_virt_3D_orient_ValidateSettings(), fsl_fxas21002_i2cspi_3D_gyro_Configure(), fsl_fxas21002_i2cspi_3D_gyro_ValidateSettings(), fsl_fxlc95000_Configure(), fsl_fxls8471_i2cspi_3D_accel_Configure(), fsl_fxls8952_i2c_3D_accel_Configure(), fsl_fxls8952_i2c_3D_accel_ValidateSettings(), fsl_fxos8700_i2cspi_6D_AccMag_Configure(), fsl_fxos8700_i2cspi_6D_AccMag_ValidateSettings(), fsl_mag3110_i2c_3D_mag_Configure(), fsl_mma8491q_i2c_3D_accel_Configure(), fsl_mma865x_i2c_3D_accel_Configure(), fsl_mma955x_Configure(), fsl_mpl3115_i2c_1D_press_Configure(), fxls8471_GetConfig(), mag3110_SetConfig(), mag3110_ValidateConfig(), mma865x_GetConfig(), mpl3115_SetConfig(), and mpl3115_ValidateConfig().
| isf_fifo_t* pSampleBufferInfo |
information about the data buffer for sample data
Definition at line 81 of file isf_dsa_adapter.h.
Referenced by Analog_1_fsl_Sensor_Generic_AnalogCallback(), configure_sensor(), Custom_1_fsl_Sensor_Custom_PeriodicCallback(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxlc95000_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxls8952_i2c_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma8491q_read_data_OneShotCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mma955x_PeriodicCallback(), and fsl_mpl3115_i2c_1D_press_PeriodicCallback().
| isf_dsa_result_types_t resultFormat |
The format of data to be returned- RAW, FIXED, FLOAT
Definition at line 84 of file isf_dsa_adapter.h.
Referenced by Analog_1_fsl_Sensor_Generic_AnalogCallback(), configure_sensor(), Custom_1_fsl_Sensor_Custom_PeriodicCallback(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fusion_virt_3D_orient_ValidateSettings(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxlc95000_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxls8952_i2c_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma8491q_read_data_OneShotCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mma955x_PeriodicCallback(), and fsl_mpl3115_i2c_1D_press_PeriodicCallback().
| isf_SensorDataTypes_t resultType |
The desired data type to be returned
Definition at line 83 of file isf_dsa_adapter.h.
Referenced by Analog_1_fsl_Sensor_Generic_AnalogCallback(), configure_sensor(), Custom_1_fsl_Sensor_Custom_PeriodicCallback(), fsl_fusion_virt_3D_orient_PeriodicCallback(), fsl_fusion_virt_3D_orient_ValidateSettings(), fsl_fxas21002_i2cspi_3D_gyro_PeriodicCallback(), fsl_fxlc95000_PeriodicCallback(), fsl_fxls8471_i2cspi_3D_accel_PeriodicCallback(), fsl_fxls8952_i2c_3D_accel_PeriodicCallback(), fsl_fxos8700_i2cspi_6D_AccMag_PeriodicCallback(), fsl_mag3110_i2c_3D_mag_PeriodicCallback(), fsl_mma8491q_read_data_OneShotCallback(), fsl_mma865x_i2c_3D_accel_PeriodicCallback(), fsl_mma955x_PeriodicCallback(), and fsl_mpl3115_i2c_1D_press_PeriodicCallback().