![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines the dummy DSA data buffer format. More...
#include <fsl_mag3110_i2c_3D_mag.h>

Data Fields | |
| uint32 | timeStamp |
| int16 | mag [3] |
| uint8 | addr |
This structure defines the dummy DSA data buffer format.
Definition at line 23 of file fsl_mag3110_i2c_3D_mag.h.
| uint8 addr |
The device "address" can uniquely identify the sensor
Definition at line 26 of file fsl_mag3110_i2c_3D_mag.h.
Referenced by fsl_mag3110_i2c_3D_mag_Initialize().
| int16 mag[3] |
The magnetometer data
Definition at line 25 of file fsl_mag3110_i2c_3D_mag.h.
Referenced by fsl_mag3110_i2c_3D_mag_Initialize(), and fsl_mag3110_i2c_3D_mag_PeriodicCallback().
| uint32 timeStamp |
The time stamp for the data packet.
Definition at line 24 of file fsl_mag3110_i2c_3D_mag.h.
Referenced by fsl_mag3110_i2c_3D_mag_Initialize(), and fsl_mag3110_i2c_3D_mag_PeriodicCallback().