![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines important settings. More...
#include <fsl_mma865x_i2c_3D_accel.h>

Data Fields | |
| uint8 | sampleRateIndex |
| Holds the ODR index into the rate array fsl_mma865x_period */. More... | |
This structure defines important settings.
Definition at line 49 of file fsl_mma865x_i2c_3D_accel.h.
| uint8 sampleRateIndex |
Holds the ODR index into the rate array fsl_mma865x_period */.
Definition at line 51 of file fsl_mma865x_i2c_3D_accel.h.
Referenced by mma865x_GetConfig(), and mma865x_SetConfig().