![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
#include <fsl_mma955x_i2cspi_pedo.h>

Definition at line 41 of file fsl_mma955x_i2cspi_pedo.h.
| dm_ChannelDescriptor_t cDescriptor |
Device Messaging channel descriptor
Definition at line 42 of file fsl_mma955x_i2cspi_pedo.h.
Referenced by fsl_mma955x_Initialize().
| dm_DeviceDescriptor_t deviceHandle |
Device messaging device handle.
Definition at line 43 of file fsl_mma955x_i2cspi_pedo.h.
Referenced by fsl_mma955x_Configure(), fsl_mma955x_EndData(), fsl_mma955x_Initialize(), fsl_mma955x_Shutdown(), fsl_mma955x_StartData(), mma955x_GetConfig(), mma955x_GetData(), mma955x_GetPedometerData(), mma955x_ValidateConfig(), and mma955x_WriteConfig().
| LWSEM_STRUCT deviceSemaphore |
Task synchronization mechanism for this data structure.
Definition at line 44 of file fsl_mma955x_i2cspi_pedo.h.
Referenced by fsl_mma955x_Configure(), fsl_mma955x_EndData(), fsl_mma955x_Initialize(), fsl_mma955x_PeriodicCallback(), and fsl_mma955x_StartData().
| mma955x_appConfigRegister_t localCfgBuffer |
Hold a local copy of the mma955x App config registers
Definition at line 47 of file fsl_mma955x_i2cspi_pedo.h.
Referenced by fsl_mma955x_Initialize().
| uint8 localCfgBufSize |
Number of bytes on the localCfgBuffer array
Definition at line 48 of file fsl_mma955x_i2cspi_pedo.h.
| mma955x_DataBuffer_t* pCurrentSample |
Holds the most recently read sample
Definition at line 46 of file fsl_mma955x_i2cspi_pedo.h.
Referenced by fsl_mma955x_Initialize(), and fsl_mma955x_PeriodicCallback().
| uint8 tempReadBuffer[32] |
scratch buffer for result of miscellaneous reads
Definition at line 49 of file fsl_mma955x_i2cspi_pedo.h.
| bm_callback_token_t token |
Bus Manager handle
Definition at line 45 of file fsl_mma955x_i2cspi_pedo.h.
Referenced by fsl_mma955x_Configure(), fsl_mma955x_EndData(), fsl_mma955x_Shutdown(), and fsl_mma955x_StartData().