![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
rli application configuration buffer format. More...

Data Fields | |
| uint8 | device |
| uint8 | channel |
| uint8 | error |
rli application configuration buffer format.
Definition at line 69 of file rli_project.c.
| uint8 channel |
Definition at line 71 of file rli_project.c.
Referenced by device_connect(), and device_disconnect().
| uint8 device |
Definition at line 70 of file rli_project.c.
Referenced by device_connect(), device_disconnect(), and rli_ci_app_callback().
| uint8 error |
Definition at line 72 of file rli_project.c.
Referenced by rli_ci_app_callback(), and rli_PeriodicCallback().