![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines the spi slave command format. More...
#include <isf_spi_master_types.h>

Data Fields | |
| uint32 | size |
| uint8 * | pReadBuffer |
| uint8 * | pWriteBuffer |
This structure defines the spi slave command format.
Definition at line 36 of file isf_spi_master_types.h.
| uint8* pReadBuffer |
The handle the readbuffer.
Definition at line 40 of file isf_spi_master_types.h.
Referenced by fsl_95000_spi_slave_read_postprocess(), fsl_95000_spi_slave_read_preprocess(), fsl_95000_spi_slave_write_preprocess(), fsl_955x_spi_slave_read_postprocess(), fsl_955x_spi_slave_read_preprocess(), fsl_955x_spi_slave_write_preprocess(), fsl_gauss_spi_slave_read_postprocess(), fsl_gauss_spi_slave_read_preprocess(), fsl_gauss_spi_slave_write_preprocess(), fsl_leon_spi_slave_read_postprocess(), fsl_leon_spi_slave_read_preprocess(), fsl_leon_spi_slave_write_preprocess(), fsl_veryon_spi_slave_read_postprocess(), fsl_veryon_spi_slave_read_preprocess(), fsl_veryon_spi_slave_write_preprocess(), rli_spi_slave_read_postprocess(), rli_spi_slave_read_preprocess(), and rli_spi_slave_write_preprocess().
| uint8* pWriteBuffer |
The handle the writecommand.
Definition at line 41 of file isf_spi_master_types.h.
Referenced by fsl_95000_spi_slave_read_preprocess(), fsl_95000_spi_slave_write_preprocess(), fsl_955x_spi_slave_read_preprocess(), fsl_955x_spi_slave_write_preprocess(), fsl_gauss_spi_slave_read_preprocess(), fsl_gauss_spi_slave_write_preprocess(), fsl_leon_spi_slave_read_preprocess(), fsl_leon_spi_slave_write_preprocess(), fsl_veryon_spi_slave_read_preprocess(), fsl_veryon_spi_slave_write_preprocess(), rli_spi_slave_read_preprocess(), and rli_spi_slave_write_preprocess().
| uint32 size |
The tranfer size.
Definition at line 39 of file isf_spi_master_types.h.
Referenced by fsl_95000_spi_slave_read_postprocess(), fsl_95000_spi_slave_read_preprocess(), fsl_95000_spi_slave_write_preprocess(), fsl_955x_spi_slave_read_postprocess(), fsl_955x_spi_slave_read_preprocess(), fsl_955x_spi_slave_write_preprocess(), fsl_gauss_spi_slave_read_postprocess(), fsl_gauss_spi_slave_read_preprocess(), fsl_gauss_spi_slave_write_preprocess(), fsl_leon_spi_slave_read_postprocess(), fsl_leon_spi_slave_read_preprocess(), fsl_leon_spi_slave_write_preprocess(), fsl_veryon_spi_slave_read_postprocess(), fsl_veryon_spi_slave_read_preprocess(), fsl_veryon_spi_slave_write_preprocess(), rli_spi_slave_read_postprocess(), rli_spi_slave_read_preprocess(), and rli_spi_slave_write_preprocess().