![]() |
ISF
2.2 rev 5
Intelligent Sensing Framework for Kinetis with Processor Expert
|
This structure defines a device endpoint encapsulation for uart handler. More...
#include <isf_uart_adapter.h>

Data Fields | |
| busHandle_t * | pBusHandle |
This structure defines a device endpoint encapsulation for uart handler.
Definition at line 23 of file isf_uart_adapter.h.
| busHandle_t* pBusHandle |
The pointer to the bus handle.
Definition at line 25 of file isf_uart_adapter.h.
Referenced by uart_adapter_get_endpoint(), uart_adapter_read(), and uart_adapter_write().