=============================================================================
List of generated methods in project: PE_LL64_Demo

THIS TEXT DESCRIPTION IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
=============================================================================

Module "LCD1"      (bean Init_LCD_HCS08)
   - LCD1_Init -This method initializes registers of the LCD module according to this Peripheral Initialization Bean settings. 
                Call this method in the user code to initialize the module. By default, the method is called by PE 
                automatically; see "Call Init method" property of the bean for more details.

Module "ADC1"      (bean Init_ADC_HCS08)
   - ADC1_Init -This method initializes registers of the ADC module according to this Peripheral Initialization Bean settings. 
                Call this method in user code to initialize the module. By default, the method is called by PE automatically; 
                see "Call Init method" property of the bean for more details.

Module "LED2"      (bean BitIO)
   - LED2_GetVal -Returns the input/output value. If the direction is [input] then the input value of the pin is read and 
                returned. If the direction is [output] then the last written value is returned (see <Safe mode> property for 
                limitations). This method cannot be disabled if direction is [input].
   - LED2_PutVal -The specified output value is set. If the direction is [input], the bean saves the value to a memory or a 
                register and this value will be written to the pin after switching to the output mode (using [SetDir(TRUE)]; 
                see <Safe mode> property for limitations). If the direction is [output], it writes the value to the pin. 
                (Method is available only if the direction = _[output]_ or _[input/output]_).
   - LED2_ClrVal -Clears (set to zero) the output value. It is equivalent to the [PutVal(FALSE)]. This method is available only 
                if the direction = _[output]_ or _[input/output]_.
   - LED2_SetVal -Sets (to one) the output value. It is equivalent to the [PutVal(TRUE)]. This method is available only if the 
                direction = _[output]_ or _[input/output]_.

Module "LED3"      (bean BitIO)
   - LED3_GetVal -Returns the input/output value. If the direction is [input] then the input value of the pin is read and 
                returned. If the direction is [output] then the last written value is returned (see <Safe mode> property for 
                limitations). This method cannot be disabled if direction is [input].
   - LED3_PutVal -The specified output value is set. If the direction is [input], the bean saves the value to a memory or a 
                register and this value will be written to the pin after switching to the output mode (using [SetDir(TRUE)]; 
                see <Safe mode> property for limitations). If the direction is [output], it writes the value to the pin. 
                (Method is available only if the direction = _[output]_ or _[input/output]_).
   - LED3_ClrVal -Clears (set to zero) the output value. It is equivalent to the [PutVal(FALSE)]. This method is available only 
                if the direction = _[output]_ or _[input/output]_.
   - LED3_SetVal -Sets (to one) the output value. It is equivalent to the [PutVal(TRUE)]. This method is available only if the 
                direction = _[output]_ or _[input/output]_.

Module "LED4"      (bean BitIO)
   - LED4_GetVal -Returns the input/output value. If the direction is [input] then the input value of the pin is read and 
                returned. If the direction is [output] then the last written value is returned (see <Safe mode> property for 
                limitations). This method cannot be disabled if direction is [input].
   - LED4_PutVal -The specified output value is set. If the direction is [input], the bean saves the value to a memory or a 
                register and this value will be written to the pin after switching to the output mode (using [SetDir(TRUE)]; 
                see <Safe mode> property for limitations). If the direction is [output], it writes the value to the pin. 
                (Method is available only if the direction = _[output]_ or _[input/output]_).
   - LED4_ClrVal -Clears (set to zero) the output value. It is equivalent to the [PutVal(FALSE)]. This method is available only 
                if the direction = _[output]_ or _[input/output]_.
   - LED4_SetVal -Sets (to one) the output value. It is equivalent to the [PutVal(TRUE)]. This method is available only if the 
                direction = _[output]_ or _[input/output]_.

Module "KB1"       (bean KBI)
   - KB1_GetVal -Returns the value of pins
   - KB1_SetEdge -Sets the sensitive edge. If all selected pins don't have the same edge setting possibility, the method allows 
                to set only those edges that are common (possible to set for all selected pins).

Module "TOD1"      (bean Init_TOD_HCS08)
   - TOD1_Init -This method initializes registers of the TOD module according to this Peripheral Initialization Bean settings. 
                Call this method in user code to initialize the module. By default, the method is called by PE automatically; 
                see "Call Init method" property of the bean for more details.

Module "IRQ1"      (bean Init_IRQ_HCS08)
   - IRQ1_Init -This method initializes registers of the IRQ module according to this Peripheral Initialization Bean settings. 
                Call this method in user code to initialize the module. By default, the method is called by PE automatically; 
                see "Call Init method" property of the bean for more details.

Module "AS1"       (bean AsynchroSerial)
   - AS1_RecvChar -If any data is received, this method returns one character, otherwise it returns an error code (it does not 
                wait for data). This method is enabled only if the receiver property is enabled.  [Note:] Because the preferred 
                method to handle error and break exception in the interrupt mode is to use events <OnError> and <OnBreak> the 
                return value ERR_RXEMPTY has higher priority than other error codes. As a consequence the information about an 
                exception in interrupt mode is returned only if there is a valid character ready to be read. Version specific 
                information for Freescale 56800 derivatives ]   DMA mode:  If DMA controller is available on the selected CPU 
                and the receiver is configured to use DMA controller then this method only sets the selected DMA channel. Then 
                the status of the DMA transfer can be checked using GetCharsInRxBuf method. See an example of a typical usage 
                for details about the communication using DMA.
   - AS1_SendChar -Sends one character to the channel. If the bean is temporarily disabled (Disable method) SendChar method 
                only stores data into an output buffer. In case of a zero output buffer size, only one character can be stored. 
                Enabling the bean (Enable method) starts the transmission of the stored data. This method is available only if 
                the transmitter property is enabled.  Version specific information for Freescale 56800 derivatives ]   DMA mode:
                If DMA controller is available on the selected CPU and the transmitter is configured to use DMA controller then 
                this method only sets selected DMA channel. Then the status of the DMA transfer can be checked using 
                GetCharsInTxBuf method. See an example of a typical usage for details about communication using DMA.
   - AS1_GetCharsInRxBuf -Returns the number of characters in the input buffer. This method is available only if the receiver 
                property is enabled. Version specific information for Freescale 56800 derivatives ]   DMA mode:  If DMA 
                controller is available on the selected CPU and the receiver is configured to use DMA controller then this 
                method returns the number of characters in the receive buffer.
   - AS1_GetCharsInTxBuf -Returns the number of characters in the output buffer. This method is available only if the 
                transmitter property is enabled. Version specific information for Freescale 56800 derivatives ]   DMA mode:  If 
                DMA controller is available on the selected CPU and the transmitter is configured to use DMA controller then 
                this method returns the number of characters in the transmit buffer.

Module "ACCEL_SLEEP_B" (bean BitIO)
   - ACCEL_SLEEP_B_SetDir -Sets a pin direction (available only if the direction = _[input/output]_).
   - ACCEL_SLEEP_B_GetVal -Returns the input/output value. If the direction is [input] then the input value of the pin is read 
                and returned. If the direction is [output] then the last written value is returned (see <Safe mode> property 
                for limitations). This method cannot be disabled if direction is [input].
   - ACCEL_SLEEP_B_PutVal -The specified output value is set. If the direction is [input], the bean saves the value to a memory 
                or a register and this value will be written to the pin after switching to the output mode (using 
                [SetDir(TRUE)]; see <Safe mode> property for limitations). If the direction is [output], it writes the value to 
                the pin. (Method is available only if the direction = _[output]_ or _[input/output]_).
   - ACCEL_SLEEP_B_ClrVal -Clears (set to zero) the output value. It is equivalent to the [PutVal(FALSE)]. This method is 
                available only if the direction = _[output]_ or _[input/output]_.
   - ACCEL_SLEEP_B_SetVal -Sets (to one) the output value. It is equivalent to the [PutVal(TRUE)]. This method is available 
                only if the direction = _[output]_ or _[input/output]_.

Module "BUZZER"    (bean PWM)
   - BUZZER_SetRatio16 -This method sets a new duty-cycle ratio. Ratio is expressed as a 16-bit unsigned integer number. 0 - 
                FFFF value is proportional to ratio 0 - 100%. The method is available only if it is not selected list of 
                predefined values in <Starting pulse width> property.   Note: Calculated duty depends on the timer 
                possibilities and on the selected period.
   - BUZZER_SetDutyUS -This method sets the new duty value of the output signal. The duty is expressed in microseconds as a 
                16-bit unsigned integer number. The method is available only if it is not selected list of predefined values in 
                <Starting pulse width> property.
   - BUZZER_SetDutyMS -This method sets the new duty value of the output signal. The duty is expressed in milliseconds as a 
                16-bit unsigned integer number. The method is available only if it is not selected list of predefined values in 
                <Starting pulse width> property.

Module "Cpu"       (bean MC9S08LL64_80)
   - Cpu_EnableInt -Enables maskable interrupts
   - Cpu_DisableInt -Disables maskable interrupts

===================================================================================