1
Out of the Box2
Get Software3
Plug It In4
Create Application Project5
Build and RunSign in to save your progress. Don't have an account? Create one.

The S32K344EVB-LQ100 is an evaluation board (EVB) based on the NXP S32K344 automotive microcontroller (MCU). The device features dual Arm® Cortex®-M7 cores, functional safety support up to ASIL-D, an integrated hardware security engine (HSE), advanced communication peripherals, floating-point support and low-power operating modes, making it suitable for automotive and industrial applications.
This guide will walk you through setting up the S32K344EVB-LQ100, preparing the required development tools as well as creating, configuring, building and running an application in S32 Design Studio (S32DS).
To help familiarize you with the board, the figure below labels the EVB's core components.
Something went wrong! Please try again.
To obtain the software needed to set up and use the evaluation board, you will first need to log in to NXP.com with your credentials.
In this step, you will locate the software needed for the S32K344EVB-LQ100. Go to the Automotive Software Package Manager and select "S32K3" as your device under "General Purpose MCUs."
To locate the software downloads required for this EVB, expand the menu hierarchy and navigate to the "FRDM Automotive S32K3 + S32M27 Board Installation Package" bundle. From the available components, select at least "S32 Design Studio and Configuration Tools" and "Real-Time Drivers." All other software packages in this category are optional and may be installed as needed.
Once you have selected the software components, you will click the button labeled "GENERATE BUNDLE INSTALLER" located below the drop-down menu.
Before you can use the software, you will be required to review the Export Control information and the Software License Agreement. Follow the wizard to complete the following steps:
Note: Because the NXP Multi Installer is only active for a limited time after it is generated, it is recommended that you begin the installation as soon as the download is complete.
The FRDM Automotive Board Installation Package automatically installs and configures the required software, simplifying the setup process.
Something went wrong! Please try again.
The latest version of S32 Design Studio includes the GNU Compiler Collection (GCC) v11.4 toolchain. To ensure full compatibility between the toolchain and the Real-Time Drivers (RTD), you will also need to install GCC v10.2.
To install the GCC v10.2 toolchain, select Help → S32DS Extensions and Updates from the S32 Design Studio top menu. In the S32DS Extensions and Updates dialog, locate and install GCC v10.2.
Note: Optional software is also available for download from the S32K3 Standard Software Package or S32K3 Reference Software Package. In S32DS, go to Help → S32DS Extensions and Updates from the top menu to open the S32DS Extensions and Updates dialogue where you click on Add Update Sites link. Or use drag and drop option - just drag downloaded updatesite file and drop on S32DS Extensions and Updates menu. Added sw package will be also automatically selected for following installation. Refer to the screenshots above and below for examples.
Something went wrong! Please try again.
In this step, to prepare the board for use you will connect the S32K344EVB-LQ100 evaluation board to your computer and power it on.
Refer to both the board layout image and the table below to locate the jumpers.
Table. S32K344EVB-LQ100 Default Solder Jumper Settings
| Jumper | State | Notes |
|---|---|---|
SJ1 |
1-2 | VDD_HV_A domain powered from USB |
SJ2 |
1-2 | VDD_HV_A domain voltage 5 V |
SJ3 |
1-2 | VDD_HV_B domain powered from USB |
SJ4 |
1-2 | VDD_HV_B domain voltage 3.3 V |
SJ5 |
1-2 | V15_MCU domain powered via external NPN ballast transistor from VDD_HV_B domain |
SJ6 |
1-2 | TJA1057 CAN Transceiver powered from VDD_HV_A domain |
Something went wrong! Please try again.
Next, you will power the board by connecting a USB Type-C to the J1 connector.
Three orange LEDs indicates the presence of the VDD_HV_A and VDD_HV_B supply voltages, and that the S32K3 debug interface is ready.
You also have the option to program the S32K3 MCU using the 10-pin Arm Cortex Debug Connector. To use this option,
connect an external debug interface to connector J4, located above the S32K3 MCU.
Something went wrong! Please try again.
In this step, you will use S32DS to create and configure an application project for the S32K344EVB-LQ100 EVB.
Something went wrong! Please try again.
PTA13 pin, which is connected to the green LED, as a GPIO outputNote: PTA14 = Blue LED; PTE2 = Red LED
PTA13 (without spaces), such as GREEN_LEDSomething went wrong! Please try again.
Siul2_Dio driver to the applicationSomething went wrong! Please try again.
/* Including necessary configuration files. */
#include "Mcal.h"
#include "Siul2_Port_Ip.h"
#include "Siul2_Dio_Ip.h"
volatile int exit_code = 0;
/* User includes */int main(void)
{
/* Write your code here */
Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals,g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals);
for(;;)
{
}
return exit_code;
}Note: While editing the code, you may use shortcuts: Pressing CTRL + Space generates a list of the available functions or arguments. Also, remember to include a semicolon at the end of your line of code.
GREEN_LED pinint main(void)
{
/* Write your code here */
Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals,g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals);
for(;;)
{
Siul2_Dio_Ip_TogglePins(GREEN_LED_PORT, 1<<(GREEN_LED_PIN));
} return exit_code; }Something went wrong! Please try again.
Now, you will take your S32K344EVB-LQ100 EVB for a test drive. Follow the instructions in each subsection to build the application, upload it to the S32K344 and also debug the code in S32 Design Studio.
Open the Debug Configurations menu, then select one of the predefined debug configurations to build the application and upload it to the S32K344 microcontroller (MCU).
Something went wrong! Please try again.
S32 Design Studio switches to the Debug perspective. Select Step Over or press F6 to step through the code.
The green LED should now be toggling in a continuous loop.
Something went wrong! Please try again.
Similar to the "Edit Code" step in the previous section, you may update the code for clock initialization.
/* Including necessary configuration files. */
#include "Mcal.h"
#include "Siul2_Port_Ip.h"
#include "Siul2_Dio_Ip.h"
#include "Clock_Ip.h"
volatile int exit_code = 0;
/* User includes */
int main(void)
{
Clock_Ip_StatusType ClockStatus;
ClockStatus = Clock_Ip_Init(&Clock_Ip_aClockConfig[0]);
/* Write your code here */
Siul2_Port_Ip_Init(NUM_OF_CONFIGURED_PINS_PortContainer_0_BOARD_InitPeripherals,
g_pin_mux_InitConfigArr_PortContainer_0_BOARD_InitPeripherals);
for(;;)
{
Siul2_Dio_Ip_TogglePins(GREEN_LED_PORT, 1<<(GREEN_LED_PIN));
}
return exit_code;
}Something went wrong! Please try again.
The resources listed below have been curated to support you through the evaluation and development process.
Select Software Packages from Automotive Software Package Manager
Add GCC Toolchain Version 10.2
Check the Default Solder Jumper Positions in the S32K344EVB-LQ100 EVB
Plug In the Power Supply and S32K3 Debug Interface