=============================================================================
List of generated methods in project: main

THIS TEXT DESCRIPTION IS GENERATED BY THE TOOL. DO NOT MODIFY IT.
=============================================================================

Module "DAC"       (component Init_DAC_56800)
   - DAC_Init -This method initializes registers of the DAC module according to this Peripheral Initialization settings. Call 
                this method in the user code to initialize the module. By default, the method is called by PE automatically; 
                see <Call Init method> property of the component for more details.

Module "CMPD"      (component Init_HSCMP_VAR0)
   - CMPD_Init -This method initializes registers of the HSCMP module according to the Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "PWMA"      (component Init_eFlexPWM_56800)
   - PWMA_Init -This method initializes registers of the eFlexPWM module according to the Peripheral Initialization settings. 
                Call this method in user code to initialize the module. By default, the method is called by PE automatically; 
                see "Call Init method" property of the component for more details.

Module "Cpu"       (component MC56F84789VLL)
   - Cpu_EnableInt -Enables all maskable interrupts
   - Cpu_DisableInt -Disables all maskable interrupts
   - Cpu_SetWaitMode -Sets low power mode - Wait mode.   For more information about the wait mode see this CPU documentation.   
                Release from wait mode: Reset or interrupt
   - Cpu_SetStopMode -Sets low power mode - Stop mode.   For more information about the stop mode see this CPU documentation.

===================================================================================