![]() |
Component Library:Sensor Driver for NMH1000
v1.0
Platform agnostic sensor driver interfaces for NMH1000 sensor
|
#include <nmh1000_regdef.h>

Data Fields | |
| struct { | |
| uint8_t out_b: 1 | |
| uint8_t rst_stat: 1 | |
| uint8_t _reserved_: 1 | |
| uint8_t opmode: 1 | |
| uint8_t _reserved_1: 1 | |
| uint8_t mdr: 1 | |
| uint8_t mdo: 1 | |
| uint8_t output: 1 | |
| } | b |
| uint8_t | w |
Definition at line 61 of file nmh1000_regdef.h.
| uint8_t _reserved_ |
Definition at line 68 of file nmh1000_regdef.h.
| uint8_t _reserved_1 |
Definition at line 72 of file nmh1000_regdef.h.
| struct { ... } b |
| uint8_t mdo |
Definition at line 76 of file nmh1000_regdef.h.
| uint8_t mdr |
Definition at line 73 of file nmh1000_regdef.h.
| uint8_t opmode |
Definition at line 69 of file nmh1000_regdef.h.
| uint8_t out_b |
Definition at line 63 of file nmh1000_regdef.h.
| uint8_t output |
Definition at line 79 of file nmh1000_regdef.h.
| uint8_t rst_stat |
Definition at line 66 of file nmh1000_regdef.h.
| uint8_t w |
Definition at line 82 of file nmh1000_regdef.h.