/************************************************************************
* (c) Copyright Freescale Semiconductor, Inc 2012, All Rights Reserved  *
************************************************************************/

/************************************************************************
*             EEE Calculator for C55 Microcontroller Family             *
*                                                                       *
*   FILE NAME     :  readme.txt                                         *
*   DATE          :  Nov 26 2012                                        *
*   AUTHOR        :  FPT Team                                           *
*   EMAIL         :  r56611@freescale.com                               *
*************************************************************************/

/****************************** CHANGES *********************************
* 0.5.0   07.30.2009	     Pavan KUmar         Final Release Version.
* 0.5.4   11.26.2012	     FPT Team            Updated version.
*************************************************************************/

Description.

This folder contains the MSI excutable for the C55 EEE calculator.
For installing the application just double click on the MSI file(C55_EEE_Calc.msi)
and follow the instructions.
The application can be opened from the ICON(C55_EEE_Calc)which appears on 
the desktop after installation.

System Requirements:

Windows XP, SP2.

Note:
If there is an ERROR message "The application failed to start because the application 
configuration is incorrect",
Please install "Visual C++ 2005 Redistributable Package (x86)" provided as a part of the 
release package.