/************************************************************************
* (c) Copyright Freescale Semiconductor, Inc 2012, All Rights Reserved  *
************************************************************************/

/************************************************************************
*            EEE Calculator for C90TFS Microcontroller Family           *
*                                                                       *
*   FILE NAME     :  readme.txt                                         *
*   DATE          :  Dec 07, 2012                                       *
*   AUTHOR        :  FPT Team                                           *
*   EMAIL         :  r56611@freescale.com                               *
*************************************************************************/

/****************************** CHANGES *********************************
* 0.1.0   12.07.2012	     FPT Team         Release Version.
*************************************************************************/

Description.

This folder contains the MSI excutable for the C90TFS EEE calculator.
For installing the application just double click on the MSI file(C90TFS_EEECalculator.msi)
and follow the instructions.
The application can be opened from the ICON (C90TFS_EEE_Calc.exe) which appears on 
the desktop after installation.

System Requirements:

Windows XP, SP2.

Note:
If there is an ERROR message "The application failed to start because the application 
configuration is incorrect",
Please install "Visual C++ 2005 Redistributable Package (x86)" provided as a part of the 
release package.