To compile this you need:

1.) The Qt Library (included if you have KDE - you need the Library and the includes to compile programs. I used v2.3 and I don't know how compatible this is with v2.2 or v3.0)

2.) the BDM driver included with gdb for bdm together with the BDMlib.

3.) gcc (g++) , make, ... 

a simple "make" hopefully builds BDMFlasher and the command line flasher clf.

type "make clf" for the command line flasher only.

To use it you need:

1.) a working mcf5272C3 or Sentec Cobra Target

2.) a working /dev/bdm device

Attention:

If BDMFlasher can not connect, there is an Error Message and the User
Interface comes up as normal. This is because this is still under constuction
and I prefer to debug the Graphical User Interface without killing my flash
contents a thousand times. Don't expect reasonable results from flashing just
because the GUI works.
If an error message comes up during start there is definitely something going
wrong.

Usage:
type clf -h for info on clf

BDMFlasher once compiled hopefully is self-explaining (I hope so, otherwise
it would be rather useless.)

rgds.
H. Craubner