//PF5300 - OTP Editor
//file generated on Mon May 4 10:19:26 2026
//Device Type : QM
//OTP ID : AL
//Part Marking : MPF5300BMMALES
//Customer : NXP

DATA FORMAT : HEX Address , Decimal Value , HEX Value

MAIN_VOTP
0x1D,3,0x03

MAIN_OTP
0x20,0,0x00
0x21,0,0x00
0x22,128,0x80
0x23,0,0x00
0x24,43,0x2b
0x25,132,0x84
0x26,0,0x00
0x27,120,0x78
0x28,9,0x09
0x29,7,0x07
0x2A,140,0x8c
0x2B,0,0x00
0x2C,54,0x36
0x2D,54,0x36
0x2E,7,0x07
0x2F,19,0x13
0x30,3,0x03
0x31,252,0xfc
0x32,1,0x01
0x33,0,0x00
0x34,119,0x77
0x35,0,0x00
0x36,0,0x00
0x37,20,0x14
0x38,0,0x00
0x39,0,0x00