//PF5300 - OTP Editor
//file generated on Mon May 4 10:12:35 2026
//Device Type : Industrial
//OTP ID : AA
//Part Marking : MPF5302BVNAAEP
//Customer : NXP

DATA FORMAT : HEX Address , Decimal Value , HEX Value

MAIN_VOTP
0x1D,5,0x05

MAIN_OTP
0x20,1,0x01
0x21,0,0x00
0x22,0,0x00
0x23,0,0x00
0x24,32,0x20
0x25,132,0x84
0x26,0,0x00
0x27,120,0x78
0x28,6,0x06
0x29,7,0x07
0x2A,120,0x78
0x2B,30,0x1e
0x2C,84,0x54
0x2D,84,0x54
0x2E,102,0x66
0x2F,3,0x03
0x30,5,0x05
0x31,252,0xfc
0x32,0,0x00
0x33,0,0x00
0x34,247,0xf7
0x35,58,0x3a
0x36,0,0x00
0x37,10,0x0a
0x38,0,0x00
0x39,0,0x00