//PF5300 - OTP Editor
//file generated on Thu May 14 08:31:55 2026
//Device Type : (Inc_VR5510)-QM
//OTP ID : A1
//Part Marking : PPF53BDBMMA1ES
//Customer : NXP

DATA FORMAT : HEX Address , Decimal Value , HEX Value

MAIN_VOTP
0x1D,3,0x03

MAIN_OTP
0x20,0,0x00
0x21,0,0x00
0x22,128,0x80
0x23,0,0x00
0x24,43,0x2b
0x25,4,0x04
0x26,0,0x00
0x27,112,0x70
0x28,9,0x09
0x29,6,0x06
0x2A,140,0x8c
0x2B,0,0x00
0x2C,60,0x3c
0x2D,0,0x00
0x2E,0,0x00
0x2F,19,0x13
0x30,6,0x06
0x31,252,0xfc
0x32,1,0x01
0x33,0,0x00
0x34,0,0x00
0x35,0,0x00
0x36,0,0x00
0x37,1,0x01
0x38,0,0x00
0x39,0,0x00