Expert Mode Data File // How to read, Write and connect to bus 0 or bus 1 or both using PCA9545A; 4-channels I2C-bus switch and interrupt and reset logic // Board: Fm+ demo board OM13260, board OM13495 TSSOP20 with PCA9545A installed // Connectivity: Connect Fm+ I2C bus1 to SDA and SCL, Set A1 pin to GND and A0 to Pull-up; the slave device address = 0xE2; // Connect Reset pin to pull-up // I2C Write Protocol : |S|Addr + W|A|Data|A|P| // I2C Read Protocol : |S|Addr + R|A|Data|NACK|P| //---------------------------------------------------------- // Expert sw format: // slave addr,Read/Write,stop bit = yes/No,delay ms,data,comments: notes //---------------------------------------------------------- // dumy read for user to read this file E3,Read,Yes,00,00,Comments: Please read this file before run. use text editor to open //Start program //write cycle; write to CONTROL resgister to connect master to channel 0 only E2,Write,Yes,00,01,Comments: Write addr 0xE2 with data 0x01. Master makes connection to channel 0 only // Read control register; The value should be 0x01 E2,Read,Yes,00,FF,Comments: read control register, the value should be 0x01 if the the master connected to channel 0 only //write cycle; Master connects to channel 1 and disconnects channel 0 E2,Write,Yes,00,02,Comments: Write addr 0xE2, with value 0x02; master connects ch1 only //write cycle; Master connects to all channels (channel 0,1,2 and 3)at the sam time E2,Write,Yes,00,0F,Comments: Write addr 0xE2, with value 0x0F; master connects to all channels