==============================================================================
Readme - Firmware Binary Package for CL RD710
==============================================================================

1. Document purpose

This document describes the content of the Firmware Binary of
the CL RD710 as well as known problems and restrictions.
A separate User Manual describes the first steps how to use the software in
combination with the Hardware.


2. Known problems and restrictions

* Restrictions
The Software is restricted to the CDRD 710 Hardware. The API is intended for the NXP contactless/contact reader ICs, 
as such the API is not to be ported to any technology from any other vendor.
The Software is running on a MFRC523 controller from NXP. 
NXP will not support porting to any other vendor platform. 

* Known Problems

  - None
	
3. Content


EULA.pdf (EULA - End User License Agreement)

\CLRD710_Firmware_v2_2_8
	pegoda2x.bin (Ready to Flash binary of Firmware Version 2.2.8, 
			for Information on how to update the Firmware please refer to AN10992 Quick Start Up Guide Pegoda, located as written in section 4)

FW_v2_2_8_Release_Notes.pdf (Release Notes and Update recommendation for Firmware Version 2.2.8)

Readme.txt (this document)

4. Documentation material, not included

	
All additionally available documentation can be downloaded at: 
http://www.nxp.com/demoboard/MFEV710.html#documentation


5. Revision History

V2.2.8.0 (Build 11092017):
* Support for SCardControl commands from the host over PC/SC to be used in place of 
  SCardBeginTransaction / SCardEndTransaction. This change is required to open the slot with/without the card being present.