=============================================================================
List of generated methods in project: DEVKIT-S12ZVL_lab1

This text description is generated by Processor Expert. Do not modify it.
=============================================================================

Module "P"         (component Init_GPIO_HCS12Z)
   - P_Init -This method initializes registers of the GPIO module according to the Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "Cpu"       (component MC9S12ZVL32_48)
   - Cpu_EnableInt -Enable maskable interrupts
   - Cpu_DisableInt -Disable maskable interrupts
   - Cpu_SetWaitMode -Set low power mode - Wait mode.   For more information about the wait mode see documentation of this CPU. 
                Release from Wait mode: Reset or interrupt
   - Cpu_SetStopMode -Set low power mode - Stop mode.   For more information about the stop mode see documentation of this CPU.

===================================================================================