=============================================================================
List of generated methods in project: DEVKIT-S12ZVL_Lab2ADC

This text description is generated by Processor Expert. Do not modify it.
=============================================================================

Module "PWM5"      (component Init_PWM_HCS12Z)
   - PWM5_Init -This method initializes registers of the PWM module according to this Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "AD1"       (component ADC)
   - AD1_Measure -This method performs one measurement on all channels that are set in the component inspector. (Note: If the 
                <number of conversions> is more than one the conversion of A/D channels is performed specified number of times.)
   - AD1_GetValue8 -This method returns the last measured values of all channels. Compared with <GetValue> method this method 
                returns more accurate result if the <number of conversions> is greater than 1 and <AD resolution> is less than 
                8 bits. In addition, the user code dependency on <AD resolution> is eliminated.
   - AD1_GetValue16 -This method returns the last measured values of all channels. Compared with <GetValue> method this method 
                returns more accurate result if the <number of conversions> is greater than 1 and <AD resolution> is less than 
                16 bits. In addition, the user code dependency on <AD resolution> is eliminated.

Module "Cpu"       (component MC9S12ZVL32_48)
   - Cpu_EnableInt -Enable maskable interrupts
   - Cpu_DisableInt -Disable maskable interrupts
   - Cpu_SetWaitMode -Set low power mode - Wait mode.   For more information about the wait mode see documentation of this CPU. 
                Release from Wait mode: Reset or interrupt
   - Cpu_SetStopMode -Set low power mode - Stop mode.   For more information about the stop mode see documentation of this CPU.

===================================================================================