=============================================================================
List of generated methods in project: DEVKIT_S12ZVL_Lab4SCI

This text description is generated by Processor Expert. Do not modify it.
=============================================================================

Module "SCI0"      (component Init_SCI_HCS12Z)
   - SCI0_Init -This method initializes registers of the SCI module according to this Peripheral Initialization settings. Call 
                this method in user code to initialize the module. By default, the method is called by PE automatically; see 
                "Call Init method" property of the component for more details.

Module "LED_RED_PP1" (component BitIO)
   - LED_RED_PP1_GetVal -Returns the input/output value. If the direction is [input] then the input value of the pin is read 
                and returned. If the direction is [output] then the last written value is returned (see <Safe mode> property 
                for limitations). This method cannot be disabled if direction is [input].
   - LED_RED_PP1_PutVal -The specified output value is set. If the direction is [input], the component saves the value to a 
                memory or a register and this value will be written to the pin after switching to the output mode (using 
                [SetDir(TRUE)]; see <Safe mode> property for limitations). If the direction is [output], it writes the value to 
                the pin. (Method is available only if the direction = _[output]_ or _[input/output]_).
   - LED_RED_PP1_ClrVal -Clears (set to zero) the output value. It is equivalent to the [PutVal(FALSE)]. This method is 
                available only if the direction = _[output]_ or _[input/output]_.
   - LED_RED_PP1_SetVal -Sets (to one) the output value. It is equivalent to the [PutVal(TRUE)]. This method is available only 
                if the direction = _[output]_ or _[input/output]_.

Module "LED_GREEN_PP3" (component BitIO)
   - LED_GREEN_PP3_GetVal -Returns the input/output value. If the direction is [input] then the input value of the pin is read 
                and returned. If the direction is [output] then the last written value is returned (see <Safe mode> property 
                for limitations). This method cannot be disabled if direction is [input].
   - LED_GREEN_PP3_PutVal -The specified output value is set. If the direction is [input], the component saves the value to a 
                memory or a register and this value will be written to the pin after switching to the output mode (using 
                [SetDir(TRUE)]; see <Safe mode> property for limitations). If the direction is [output], it writes the value to 
                the pin. (Method is available only if the direction = _[output]_ or _[input/output]_).
   - LED_GREEN_PP3_ClrVal -Clears (set to zero) the output value. It is equivalent to the [PutVal(FALSE)]. This method is 
                available only if the direction = _[output]_ or _[input/output]_.
   - LED_GREEN_PP3_SetVal -Sets (to one) the output value. It is equivalent to the [PutVal(TRUE)]. This method is available 
                only if the direction = _[output]_ or _[input/output]_.

Module "SWITCH_PP4" (component BitIO)
   - SWITCH_PP4_GetVal -Returns the input/output value. If the direction is [input] then the input value of the pin is read and 
                returned. If the direction is [output] then the last written value is returned (see <Safe mode> property for 
                limitations). This method cannot be disabled if direction is [input].

Module "SWITCH_PP7" (component BitIO)
   - SWITCH_PP7_GetVal -Returns the input/output value. If the direction is [input] then the input value of the pin is read and 
                returned. If the direction is [output] then the last written value is returned (see <Safe mode> property for 
                limitations). This method cannot be disabled if direction is [input].

Module "Cpu"       (component MC9S12ZVL32_48)
   - Cpu_EnableInt -Enable maskable interrupts
   - Cpu_DisableInt -Disable maskable interrupts
   - Cpu_SetWaitMode -Set low power mode - Wait mode.   For more information about the wait mode see documentation of this CPU. 
                Release from Wait mode: Reset or interrupt
   - Cpu_SetStopMode -Set low power mode - Stop mode.   For more information about the stop mode see documentation of this CPU.

===================================================================================