DUT implementation of the KeyStore interface.
More...
|
| | Define |
| | Definitions for DUT layer configuration.
|
| |
|
| phStatus_t | phKeyStore_DUT_Provision_Init (phKeyStore_DUT_DataParams_t *pDataParams, uint16_t wOption, uint8_t *pTransportKey_AES128, uint8_t *pTransportKey_AES256, uint8_t *pAppRootKey_AES128, uint8_t *pAppRootKey_AES256, uint8_t *pExpDecData, uint8_t *pDervMsg, uint8_t *pWrapIV) |
| | Initializes the DUT KeyStore component for Key provisioning. More...
|
| |
| void | phKeyStore_DUT_Provision_DeInit (phKeyStore_DUT_DataParams_t *pDataParams) |
| | De-Initializes PN7642 KeyStore component for Key provisioning. More...
|
| |
| phStatus_t | phKeyStore_DUT_SetConfig_Ext (phKeyStore_DUT_DataParams_t *pDataParams, uint16_t wConfig, uint8_t *pValue, uint16_t wValueLen) |
| | Set configuration parameter. More...
|
| |
| phStatus_t | phKeyStore_DUT_GetConfig_Ext (phKeyStore_DUT_DataParams_t *pDataParams, uint16_t wConfig, uint8_t *pValue, uint16_t *pValueLen) |
| | Get configuration parameter. More...
|
| |
| phStatus_t | phKeyStore_DUT_Provision_AppFixedKeys (phKeyStore_DUT_DataParams_t *pDataParams, uint8_t bKeyIndex, uint16_t wKeyType, uint8_t *pNewKey) |
| | Provision Application Fixed Keys. More...
|
| |
DUT implementation of the KeyStore interface.
◆ phKeyStore_DUT_Provision_Init()
Initializes the DUT KeyStore component for Key provisioning.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wOption | [In] Options to perform the following.
|
| [in] | pTransportKey_AES128 | [In] Array containing AES 128-Bit [16 Byte] Transport Key. Can be NULL if wOption = PH_KEYSTORE_PROVISION_APP_ROOT_KEY_PROVISION_DISABLED |
| [in] | pTransportKey_AES256 | [In] Array containing AES 256-Bit [32 Byte] Transport Key. Can be NULL if wOption = PH_KEYSTORE_PROVISION_APP_ROOT_KEY_PROVISION_DISABLED |
| [in] | pAppRootKey_AES128 | [In] Array containing AES 128-Bit [16 Byte] Application Root Key. Should not be Null. |
| [in] | pAppRootKey_AES256 | [In] Array containing AES 256-Bit [32 Byte] Application Root Key. Should not be Null. |
| [in] | pExpDecData | [In] Array containing AES 128-Bit [16 Byte] expected Decrypted data to be used while opening the Session. Should not be NULL. |
| [in] | pDervMsg | [In] Array containing derivation message. Should not be NULL.
- Derivation message to derive a wrapping key from existing Transport Key (NXP_TPT_KEY) or Application Root Key (APP_ROOT_KEY)
- Will be used while opening a session and provisioning the Keys.
- Should be 24 bytes in length.
|
| [in] | pWrapIV | [In] IV used for wrapping the key. This information will be used while provisioning the Key.
- Should be 16 bytes in length.
- If NULL, Zero IV will be used for wrapping the key.
|
◆ phKeyStore_DUT_Provision_DeInit()
De-Initializes PN7642 KeyStore component for Key provisioning.
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
◆ phKeyStore_DUT_SetConfig_Ext()
Set configuration parameter.
This interface is supported only for PN7642 hardware.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wConfig | [In] Configuration Identifier.
|
| [in] | pValue | [In] Configuration Value to update. |
| [in] | wValueLen | [In] Length of byte available in pValue buffer. |
◆ phKeyStore_DUT_GetConfig_Ext()
Get configuration parameter.
This interface is supported only for PN7642 hardware.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wConfig | [In] Configuration Identifier.
|
| [in] | pValue | [In] Configuration Value to retrieve. |
| [in] | pValueLen | [In] Length of byte available in pValue buffer. |
◆ phKeyStore_DUT_Provision_AppFixedKeys()
Provision Application Fixed Keys.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | bKeyIndex | [In] Key number of the hardware keys store to be provisioned. Keys Index will be 10h - 1Ah |
| [in] | wKeyType | [In] Key type of the key to be loaded. Should be one of the following
|
| [in] | pNewKey | [In] Pointer to the key itself. |