Definitions for SAM (AV4 and future SAM's) Key Classes. Should be used to set the ExtSET information. More...

Macros | |
| #define | PH_KEYSTORE_SAM_KEY_CLASS_HOST 0x00U |
| Configuring key entry as Host. | |
| #define | PH_KEYSTORE_SAM_KEY_CLASS_PICC 0x01U |
| Configuring key entry as PICC. | |
| #define | PH_KEYSTORE_SAM_KEY_CLASS_OFFLINE_CHANGE 0x02U |
| Configuring key entry as Offline Change. | |
| #define | PH_KEYSTORE_SAM_KEY_CLASS_OFFLINE_CRYPTO 0x04U |
| Configuring key entry as Offline Crypto. | |
| #define | PH_KEYSTORE_SAM_KEY_CLASS_OFFLINE_UPLOAD 0x05U |
| Configuring key entry as Offline Upload. | |
| #define | PH_KEYSTORE_SAM_KEY_CLASS_OFFLINE_PERSO 0x06U |
| Configuring key entry as Offline Perso. | |
Definitions for SAM (AV4 and future SAM's) Key Classes. Should be used to set the ExtSET information.