Contains Application specific implementations for various contactless cards like ULTRALIGHT, CLASSIC, Plus, DESFire and so on... More...

Modules | |
| MIFARE(R) Classic | |
| These Functions implement the MIFARE(R) Classic commands. | |
| MIFARE DESFire (R) | |
| These Functions implement the MIFARE DESFire(R) EV1 commands. | |
| MIFARE DESFire EVx | |
| These Functions implement the MIFARE DESFire EVx commands. | |
| MIFARE DESFire Light | |
| These Functions implement the MIFARE DESFire Light commands. | |
| MIFARE DUOX | |
| This is only a wrapper layer to abstract the different MIFARE DUOX implementations. With this wrapper it is possible to support more than one MIFARE DUOX implementation in parallel, by adapting this wrapper. | |
| Felica | |
| These Components implement the Felica commands. | |
| ICode | |
| Generic component that provides the command description of ICode products. | |
| MIFARE Identity | |
| These Functions implement the MIFARE Identity commands. | |
| ISO/IEC 18000-3 Mode3 | |
| These Components implement the ICODE ILT support. | |
| NTAG 42x DNA / TT | |
| These Functions implement the NTAG 42x DNA / TT commands. | |
| NTAG X DNA | |
| This is only a wrapper layer to abstract the different NTAG X DNA implementations. With this wrapper it is possible to support more than one NTAG X DNA implementation in parallel, by adapting this wrapper. | |
| MIFARE Plus (R) | |
| These Components implement the MIFARE Plus (R) commands. | |
| MIFARE Plus EVx | |
| These Components implement the MIFARE Plus (EVx, EV2, future versions) commands. | |
| MIFARE PRIME NTAG | |
| These Functions implement the MIFARE PRIME NTAG commands. | |
| MIFARE(R) Ultralight | |
| This is only a wrapper layer to abstract the different MIFARE Ultralight / NTAG implementations. With this wrapper it is possible to support more than one MIFARE Ultralight / NTAG implementation in parallel, by adapting this wrapper. | |
| Virtual Card Architecture (R) | |
| These Components implement the Virtual Card Architecture (R) commands. | |
Contains Application specific implementations for various contactless cards like ULTRALIGHT, CLASSIC, Plus, DESFire and so on...