These Components implement the MIFARE Identity Data Management related commands.
More...
|
| phStatus_t | phalMfIdentity_ReadData (void *pDataParams, uint8_t bOption, uint8_t bIns, uint8_t bFileNo, uint8_t *pOffset, uint8_t *pLength, uint8_t **ppRxdata, uint16_t *pRxdataLen) |
| | Reads data from standard data files or backup data files. More...
|
| |
| phStatus_t | phalMfIdentity_WriteData (void *pDataParams, uint8_t bOption, uint8_t bIns, uint8_t bFileNo, uint8_t *pOffset, uint8_t *pTxData, uint8_t *pTxDataLen) |
| | Writes data to standard data files or backup data files. More...
|
| |
| phStatus_t | phalMfIdentity_ReadRecords (void *pDataParams, uint8_t bCommOption, uint8_t bIns, uint8_t bFileNo, uint8_t *pRecNo, uint8_t *pRecCount, uint8_t *pRecSize, uint8_t **ppRxdata, uint16_t *pRxdataLen) |
| | Reads out a set of complete records from a Cyclic or Linear Record File. More...
|
| |
| phStatus_t | phalMfIdentity_WriteRecord (void *pDataParams, uint8_t bCommOption, uint8_t bIns, uint8_t bFileNo, uint8_t *pOffset, uint8_t *pData, uint8_t *pDataLen) |
| | Writes data to a record in a Cyclic or Linear Record File. More...
|
| |
| phStatus_t | phalMfIdentity_ClearRecordFile (void *pDataParams, uint8_t bFileNo) |
| | Resets a Cyclic or Linear Record File. More...
|
| |
These Components implement the MIFARE Identity Data Management related commands.
◆ phalMfIdentity_ReadData()
Reads data from standard data files or backup data files.
Chaining upto the size of the HAL Rx buffer is handled within this function. If more data is to be read, the user has to call this function again with bOption = PH_EXCHANGE_RXCHAINING | [one of the communication options]
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Communication settings for the file.
PH_EXCHANGE_RXCHAINING: To be Or'd with the above option flag if Chaining status is returned. |
| [in] | bIns | [In] If set, uses ISO 14443-4 chaining instead of DESFire application chaining. |
| [in] | bFileNo | [In] The file number from where the data to be read. |
| [in] | pOffset | [In] The offset from where the data should be read. Will be of 3 bytes with LSB first. If 0x10 need to be offset then it will be 10 00 00. |
| [in] | pLength | [In] The number of bytes to be read. Will be of 3 bytes with LSB first. If 0x10 bytes need to be read then it will be 10 00 00.
If complete file need to be read then it will be 00 00 00. |
| [out] | ppRxdata | [Out] The data retuned by the PICC. |
| [out] | pRxdataLen | [Out] Length of bytes available in RxData buffer. |
◆ phalMfIdentity_WriteData()
Writes data to standard data files or backup data files.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bOption | [In] Communication settings for the file.
|
| [in] | bIns | [In] If set, uses ISO 14443-4 chaining instead of DESFire application chaining. |
| [in] | bFileNo | [In] The file number from where the data to be read. |
| [in] | pOffset | [In] The offset from where the data should be written. Will be of 3 bytes with LSB first. If 0x10 need to be offset then it will be 10 00 00. |
| [in] | pTxData | [In] The data to be written to the PICC. |
| [in] | pTxDataLen | [In] The number of bytes to be written. Will be of 3 bytes with LSB first. If 0x10 bytes need to be written then it will be 10 00 00. |
◆ phalMfIdentity_ReadRecords()
Reads out a set of complete records from a Cyclic or Linear Record File.
Chaining upto the size of the HAL Rx buffer is handled within this function. If more data is to be read, the user has to call this function again with bCommOption = PH_EXCHANGE_RXCHAINING | [one of the communication options]
If TMI collection is ON, if pRecCount is zero then pRecSize is madatory parameter. If pRecSize and RecCount are zero and TMI collection is ON, then PH_ERR_INVALID_PARAMETER error returned. If TMI collection is ON; and if wrong pRecSize is provided, then wrong RecCount value will be calculated and updated for TMI collection.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bCommOption | [In] Communication settings for the file.
PH_EXCHANGE_RXCHAINING: To be Or'd with the above option flag if Chaining status is returned. |
| [in] | bIns | [In] If set, uses ISO 14443-4 chaining instead of DESFire application chaining. |
| [in] | bFileNo | [In] The file number from where the data to be read. |
| [in] | pRecNo | [In] 3 bytes LSB first. Record number of the newest record targeted, starting to count from the latest record written. |
| [in] | pRecCount | [In] 3 bytes LSB first. Number of records to be read. If 0x00 00 00, then all the records are read. |
| [in] | pRecSize | [In] The number of bytes to be read. Will be of 3 bytes with LSB first. |
| [out] | ppRxdata | [Out] The data retuned by the PICC. |
| [out] | pRxdataLen | [Out] Length of bytes available in RxData buffer. |
◆ phalMfIdentity_WriteRecord()
Writes data to a record in a Cyclic or Linear Record File.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bCommOption | [In] Communication settings for the file.
|
| [in] | bIns | [In] If set, uses ISO 14443-4 chaining instead of DESFire application chaining. |
| [in] | bFileNo | [In] The file number to which the data should be written. |
| [in] | pOffset | [In] The offset from where the data should be written. Will be of 3 bytes with LSB first. If 0x10 need to be offset then it will be 10 00 00. |
| [in] | pData | [In] The data to be written to the PICC. |
| [in] | pDataLen | [In] The number of bytes to be written. Will be of 3 bytes with LSB first. If 0x10 bytes need to be written then it will be 10 00 00. |
◆ phalMfIdentity_ClearRecordFile()
Resets a Cyclic or Linear Record File.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bFileNo | [In] The file number to be cleared. |