These Components implement the MIFARE Identity Secure Messaging related commands.
More...
|
| phStatus_t | phalMfIdentity_AuthenticateEv2 (void *pDataParams, uint8_t bFirstAuth, uint16_t wOption, uint16_t wKeyNo, uint16_t wKeyVer, uint8_t bKeyNoCard, uint8_t *pDivInput, uint8_t bDivLen, uint8_t bLenPcdCapsIn, uint8_t *bPcdCapsIn, uint8_t *bPcdCapsOut, uint8_t *bPdCapsOut) |
| | Performs an First or Non First Authentication depending upon bFirstAuth Parameter. More...
|
| |
These Components implement the MIFARE Identity Secure Messaging related commands.
◆ phalMfIdentity_AuthenticateEv2()
| phStatus_t phalMfIdentity_AuthenticateEv2 |
( |
void * |
pDataParams, |
|
|
uint8_t |
bFirstAuth, |
|
|
uint16_t |
wOption, |
|
|
uint16_t |
wKeyNo, |
|
|
uint16_t |
wKeyVer, |
|
|
uint8_t |
bKeyNoCard, |
|
|
uint8_t * |
pDivInput, |
|
|
uint8_t |
bDivLen, |
|
|
uint8_t |
bLenPcdCapsIn, |
|
|
uint8_t * |
bPcdCapsIn, |
|
|
uint8_t * |
bPcdCapsOut, |
|
|
uint8_t * |
bPdCapsOut |
|
) |
| |
Performs an First or Non First Authentication depending upon bFirstAuth Parameter.
This will be using the AES128 keys and will generate and verify the contents based on generic AES algorithm.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bFirstAuth | [In] One of the below options.
|
| [in] | wOption | [In] Diversification option can be one of
|
| [in] | wKeyNo | [In] Key number in keystore of software or SAM. |
| [in] | wKeyVer | [In] Key version in keystore of software or SAM. |
| [in] | bKeyNoCard | [In] Key number on card. |
| [in] | pDivInput | [In] Diversification input. Can be NULL. |
| [in] | bDivLen | [In] Length of diversification input max 31B. |
| [in] | bLenPcdCapsIn | [In] Length of PcdCapsIn. Always zero for following authentication |
| [in] | bPcdCapsIn | [In] PCD Capabilities. |
| [out] | bPcdCapsOut | [Out] PCD Capabilities. |
| [out] | bPdCapsOut | [Out] PD Capabilities. |