NXP Reader Library  v17.1.0.2535
Component : Sam_NonX
Collaboration diagram for Component : Sam_NonX:

Data Structures

struct  phalMfdfEVx_SamAV3_NonX_DataParams_t
 MIFARE DESFire EVx SAM NonX parameter structure
More...
 
struct  phalMfdfEVx_Sam_NonX_DataParams_t
 MIFARE DESFire EVx SAM NonX parameter structure
More...
 

Macros

#define PHAL_MFDFEVX_SAMAV3_NONX_ID   0x02U
 ID for SamAV3 Non X MF DesFire EVx layer.
 
#define PHAL_MFDFEVX_SAM_NONX_ID   0x04U
 ID for Sam Non X MF DesFire EVx layer.
 

Functions

phStatus_t phalMfdfEVx_SamAV3_NonX_Init (phalMfdfEVx_SamAV3_NonX_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV3_DataParams_t *pHalSamDataParams, void *pPalMifareDataParams, phTMIUtils_t *pTMIDataParams, uint8_t *pTmpBuffer, uint16_t wTmpBufSize)
 Initializes the DESFire EVx Sam AV3 component in Non X mode (S mode). More...
 
phStatus_t phalMfdfEVx_Sam_NonX_Init (phalMfdfEVx_Sam_NonX_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pHalSamDataParams, void *pPalMifareDataParams, phTMIUtils_t *pTMIDataParams, uint8_t *pTmpBuffer, uint16_t wTmpBufSize)
 Initializes the DESFire EVx Sam component in Non X mode (S mode). More...
 

Detailed Description

Function Documentation

◆ phalMfdfEVx_SamAV3_NonX_Init()

phStatus_t phalMfdfEVx_SamAV3_NonX_Init ( phalMfdfEVx_SamAV3_NonX_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams,
phhalHw_SamAV3_DataParams_t pHalSamDataParams,
void *  pPalMifareDataParams,
phTMIUtils_t pTMIDataParams,
uint8_t pTmpBuffer,
uint16_t  wTmpBufSize 
)

Initializes the DESFire EVx Sam AV3 component in Non X mode (S mode).

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_INVALID_DATA_PARAMSfor Invaid DataParams
PH_ERR_INVALID_PARAMETERfor invalid parameter values.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure
[in]pHalSamDataParams[In] Pointer to the HAL parameter structure of the SAM.
[in]pPalMifareDataParams[In] Pointer to Pal MIFARE parameter structure.
[in]pTMIDataParams[In] Pointer to the parameter structure for collecting TMI.
[in]pTmpBuffer[In] Temporary buffer for framing the command buffer. Should be higher than 256 bytes.
[in]wTmpBufSize[In] Size of Temporary buffer.

◆ phalMfdfEVx_Sam_NonX_Init()

phStatus_t phalMfdfEVx_Sam_NonX_Init ( phalMfdfEVx_Sam_NonX_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams,
void *  pHalSamDataParams,
void *  pPalMifareDataParams,
phTMIUtils_t pTMIDataParams,
uint8_t pTmpBuffer,
uint16_t  wTmpBufSize 
)

Initializes the DESFire EVx Sam component in Non X mode (S mode).

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_INVALID_DATA_PARAMSfor Invaid DataParams
PH_ERR_INVALID_PARAMETERfor invalid parameter values.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure
[in]pHalSamDataParams[In] Pointer to the HAL parameter structure of the SAM.
[in]pPalMifareDataParams[In] Pointer to Pal MIFARE parameter structure.
[in]pTMIDataParams[In] Pointer to the parameter structure for collecting TMI.
[in]pTmpBuffer[In] Temporary buffer for framing the command buffer. Should be higher than 256 bytes.
[in]wTmpBufSize[In] Size of Temporary buffer.