Data Structures | |
| struct | phalVca_SamAV2_CardTableEntry_t |
| Structure for IID table. More... | |
| struct | phalVca_SamAV2_KeyDuos_t |
| Structure for KeyDuo Storage. More... | |
| struct | phalVca_SamAV2_DataParams_t |
| SAM AV2 NonX AL-VCA parameter structure. More... | |
| struct | phalVca_SamAV3_NonX_DataParams_t |
| SAM AV3 NonX AL-VCA parameter structure. More... | |
Macros | |
| #define | PHAL_VCA_SAMAV2_NONX_ID 0x04 |
| ID for SamAV2_NonX Virtual Card Architecture layer. | |
| #define | PHAL_VCA_SAMAV3_NONX_ID 0x05 |
| ID for SamAV3_NonX Virtual Card Architecture layer. | |
| #define | PHAL_VCA_SAM_NONX_ID 0x06 |
| ID for Sam_NonX Virtual Card Architecture layer. | |
Functions | |
| phStatus_t | phalVca_SamAV2_NonX_Init (phalVca_SamAV2_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV2_DataParams_t *pSamHal, void *pPalMifareDataParams, uint8_t *pRndq, phalVca_SamAV2_KeyDuos_t *pKeyDuos, uint8_t bNumKeyDuos, phalVca_SamAV2_CardTableEntry_t *pCardTableStorage, uint16_t wNumCardTableStorageEntries) |
| Initialise this layer. More... | |
| phStatus_t | phalVca_SamAV3_NonX_Init (phalVca_SamAV3_NonX_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV3_DataParams_t *pSamHal, void *pPalMifareDataParams) |
| Initialise this layer. More... | |
| phStatus_t | phalVca_Sam_NonX_Init (phalVca_Sam_NonX_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pSamHal, void *pPalMifareDataParams) |
| phStatus_t phalVca_SamAV2_NonX_Init | ( | phalVca_SamAV2_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| phhalHw_SamAV2_DataParams_t * | pSamHal, | ||
| void * | pPalMifareDataParams, | ||
| uint8_t * | pRndq, | ||
| phalVca_SamAV2_KeyDuos_t * | pKeyDuos, | ||
| uint8_t | bNumKeyDuos, | ||
| phalVca_SamAV2_CardTableEntry_t * | pCardTableStorage, | ||
| uint16_t | wNumCardTableStorageEntries | ||
| ) |
Initialise this layer.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure. |
| [in] | pSamHal | [In] Pointer to the parameter structure of the Sam HAL. |
| [in] | pPalMifareDataParams | [In] Pointer to the parameter structure of the palMifare layer. |
| [in] | pRndq | [In] RndQ buffer. |
| [in] | pKeyDuos | [In] KeyDuo buffer. |
| [in] | bNumKeyDuos | [In] Number of KeyDuos. |
| [in] | pCardTableStorage | [In] Pointer to the Card Table storage for the layer. |
| [in] | wNumCardTableStorageEntries | [In] Number of possible Card table entries in the storage. |
| phStatus_t phalVca_SamAV3_NonX_Init | ( | phalVca_SamAV3_NonX_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| phhalHw_SamAV3_DataParams_t * | pSamHal, | ||
| void * | pPalMifareDataParams | ||
| ) |
Initialise this layer.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure. |
| [in] | pSamHal | [In] Pointer to the parameter structure of the Sam HAL. |
| [in] | pPalMifareDataParams | [In] Pointer to the parameter structure of the palMifare layer. |
| phStatus_t phalVca_Sam_NonX_Init | ( | phalVca_Sam_NonX_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| void * | pSamHal, | ||
| void * | pPalMifareDataParams | ||
| ) |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure. |
| [in] | pSamHal | [In] Pointer to the parameter structure of the Sam HAL. |
| [in] | pPalMifareDataParams | [In] Pointer to the parameter structure of the palMifare layer. |