NXP Reader Library  v17.1.0.2535
SAM AV2 HAL Initialization for Pegoda 2 (RD710) Reader in X (NonX) Mode

Example code to configure HAL and BAL for Pegoda 2 (RD710) reader with SAM AV2 in X mode. More...

Collaboration diagram for SAM AV2 HAL Initialization for Pegoda 2 (RD710) Reader in X (NonX) Mode:

Modules

 Sam AV2 X mode Initialization
 Example code to configure PAL 3A, 4A, 4, MIFARE to work in Sam AV2 X mode.
 

Detailed Description

Example code to configure HAL and BAL for Pegoda 2 (RD710) reader with SAM AV2 in X mode.

#define CHECK_SUCCESS(x) \
if ( (x) != PH_ERR_SUCCESS ) \
{ \
printf ( "\n\n" ); \
printf ( "An error occurred: (0x%04X)\n", (x) ); \
printf ( "Pressing any key will exit the demo.\n" ); \
_getch (); \
return 0; \
}
/* Variables */
phStatus_t wStatus = 0;
phKeyStore_Sw_KeyEntry_t aKeyEntry[0xFF];
phKeyStore_Sw_KeyVersionPair_t aKeyVersionPair[0xFF];
phKeyStore_Sw_KUCEntry_t aKeyUsageCounter[0xFF];
uint8_t aAtr[256];
uint8_t aTx_SamBuffer[512];
uint8_t aRx_SamBuffer[512];
uint8_t aSeed[8];
uint8_t aHostAuthKey[] = { 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 };
void* pBal_Generic = NULL;
void* pHal_Generic = NULL;
/* Initialize software KeyStore component. */
wStatus = phKeyStore_Sw_Init ( &stKeyStore, sizeof ( phKeyStore_Sw_DataParams_t ), aKeyEntry, 0xFF, aKeyVersionPair, 0x03,
aKeyUsageCounter, 0xFF );
CHECK_SUCCESS ( wStatus );
/* Initialize software Crypto component. */
wStatus = phCryptoSym_Sw_Init ( &stCryptoSym_Enc, sizeof ( phCryptoSym_Sw_DataParams_t ), &stKeyStore )
CHECK_SUCCESS ( wStatus );
wStatus = phCryptoSym_Sw_Init ( &stCryptoSym_Mac, sizeof ( phCryptoSym_Sw_DataParams_t ), &stKeyStore )
CHECK_SUCCESS ( wStatus );
wStatus = phCryptoSym_Sw_Init ( &stCryptoSym_Enc_PLUpload, sizeof ( phCryptoSym_Sw_DataParams_t ), &stKeyStore )
CHECK_SUCCESS ( wStatus );
wStatus = phCryptoSym_Sw_Init ( &stCryptoSym_Mac_PLUpload, sizeof ( phCryptoSym_Sw_DataParams_t ), &stKeyStore )
CHECK_SUCCESS ( wStatus );
wStatus = phCryptoSym_Sw_Init ( &stCryptoSym_Rnd, sizeof ( phCryptoSym_Sw_DataParams_t ), &stKeyStore )
CHECK_SUCCESS ( wStatus );
wStatus = phCryptoRng_Sw_Init ( &stCryptoRng_Rnd, sizeof ( phCryptoRng_Sw_DataParams_t ), &stKeyStore )
CHECK_SUCCESS ( wStatus );
/* Seed the random number generator with the given seed. */
memset ( aSeed, 0x00, 0x08 );
wStatus = phCryptoRng_Seed ( &stCryptoRng_Rnd, aSeed, sizeof ( aSeed ) );
/* Initialize the reader BAL component */
wStatus = phbalReg_PcscWin_Init ( &stBal_Rd710, sizeof ( phbalReg_PcscWin_DataParams_t ), aAtr, 256 );
CHECK_SUCCESS ( wStatus );
/* Connect to the first reader out of the list. */
wStatus = phbalReg_SetPort ( &stBal_Rd710, ( uint8_t * ) "NXP Pegoda X 0 0" );
CHECK_SUCCESS ( wStatus );
/* Open the reader port. */
wStatus = phbalReg_OpenPort ( &stBal_Rd710 );
CHECK_SUCCESS ( wStatus );
/*
* Initialize the reader HAL component.
* The initialization is performed for RC523 based reader IC. For this PHHAL_HW_SAMAV2_OPMODE_X_RC523 is used.
* If the initialization is required for RC663 based reader IC use PHHAL_HW_SAMAV2_OPMODE_X_RC663.
*/
wStatus = phhalHw_SamAV2_Init ( &stHal_SamAv2, sizeof ( phhalHw_SamAV2_DataParams_t ), &stBal_Rd710, NULL, &stKeyStore, &stCryptoSym_Enc,
&stCryptoSym_MAC, &stCryptoRng_Rng, PHHAL_HW_SAMAV2_OPMODE_X_RC523, 0x00, aTx_SamBuffer, sizeof ( aTx_SamBuffer ),
aRx_SamBuffer, sizeof ( aRx_SamBuffer ) );
CHECK_SUCCESS ( wStatus );
/* Update the generic components. */
pBal_Generic = &stBal_Rd710;
pHal_Generic = &stHal_SamAv2;
/* Initialize SAM Keystore component. */
wStatus = phKeyStore_SamAV2_Init ( &stKeyStoreSAM, sizeof ( phKeyStore_SamAV2_DataParams_t ), &stHal_SamAv2 );
CHECK_SUCCESS ( wStatus );
/* Detect SAM settings. This will update the Host version internally. MUST to be CALLED. */
wStatus = phhalHw_SamAV2_DetectMode ( &stHal_SamAv2 );
CHECK_SUCCESS ( wStatus );
/* Load a the key to software keystore for SAM HOST Authentication. */
wStatus = phKeyStore_FormatKeyEntry ( &stKeyStore, 0x00, PH_KEYSTORE_KEY_TYPE_AES128 );
CHECK_SUCCESS ( wStatus );
wStatus = phKeyStore_SetKeyAtPos ( &stKeyStore, 0x00, 0x00, PH_KEYSTORE_KEY_TYPE_AES128, aHostAuthKey, 0x00 );
CHECK_SUCCESS ( wStatus );
/* Perform HOST AUTHENTICATION in PLAIN mode. */
wStatus = phhalHw_SamAV2_Cmd_SAM_AuthenticateHost ( &stHal_SamAv2, 0x00, 0x00, 0x00, 0x00, 0x00, NULL, 0x00 );
CHECK_SUCCESS ( wStatus );
/* Perform Reader IC initialization. */
wStatus = phhalHw_SamAV2_Cmd_RC_Init ( &stHal_SamAv2, 0x00 );
CHECK_SUCCESS ( wStatus );
phbalReg_PcscWin_DataParams_t
PCSC (Windows) BAL parameter structure.
Definition: phbalReg.h:600
phKeyStore_Sw_Init
phStatus_t phKeyStore_Sw_Init(phKeyStore_Sw_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phKeyStore_Sw_KeyEntry_t *pKeyEntries, uint16_t wNoOfKeyEntries, phKeyStore_Sw_KeyVersionPair_t *pKeyVersionPairs, uint16_t wNoOfVersionPairs, phKeyStore_Sw_KUCEntry_t *pKUCEntries, uint16_t wNoOfKUCEntries)
Initializes the KeyStore component as software component.
phCryptoSym_Sw_Init
phStatus_t phCryptoSym_Sw_Init(phCryptoSym_Sw_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pKeyStoreDataParams)
Initialize the CryptoSym with Software as sub-component.
phKeyStore_SamAV2_DataParams_t
Sam parameter structure.
Definition: phKeyStore.h:299
phKeyStore_Sw_KeyEntry_t
Software KeyEntry structure.
Definition: phKeyStore.h:66
phKeyStore_Sw_DataParams_t
Software parameter structure.
Definition: phKeyStore.h:82
phKeyStore_SetKeyAtPos
phStatus_t phKeyStore_SetKeyAtPos(void *pDataParams, uint16_t wKeyNo, uint16_t wPos, uint16_t wKeyType, uint8_t *pNewKey, uint16_t wNewKeyVersion)
Change a symmetric key entry at the specified position.
phKeyStore_Sw_KeyVersionPair_t
Software KeyVersionPair structure for Symmetric and ASymmetric keys.
Definition: phKeyStore.h:51
phStatus_t
uint16_t phStatus_t
phcsBfl_Status_t is a signed short value, using the positive range.
Definition: ph_TypeDefs.h:158
PH_KEYSTORE_KEY_TYPE_AES128
#define PH_KEYSTORE_KEY_TYPE_AES128
AES 128 Key [16].
Definition: phKeyStore.h:1067
phCryptoRng_Sw_Init
phStatus_t phCryptoRng_Sw_Init(phCryptoRng_Sw_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pCryptoDataParams)
Initialize the CryptoRng with software as sub-component.
phhalHw_SamAV2_Cmd_RC_Init
phStatus_t phhalHw_SamAV2_Cmd_RC_Init(phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t bLoadReg)
Initialize the RC522 with a given register value set.
phKeyStore_SamAV2_Init
phStatus_t phKeyStore_SamAV2_Init(phKeyStore_SamAV2_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_SamAV2_DataParams_t *pHalDataParams)
Initializes the KeyStore component as SAM AV2 component.
phCryptoSym_Sw_DataParams_t
Data structure for Symmetric Crypto Software layer implementation.
Definition: phCryptoSym.h:435
phbalReg_SetPort
phStatus_t phbalReg_SetPort(void *pDataParams, uint8_t *pPortName)
Select Port to be used.
phKeyStore_Sw_KUCEntry_t
Software KeyUsageCounter structure.
Definition: phKeyStore.h:75
phhalHw_SamAV2_DetectMode
phStatus_t phhalHw_SamAV2_DetectMode(phhalHw_SamAV2_DataParams_t *pDataParams)
Detect UID, AV1/AV2 mode and HostAuth settings.
phCryptoRng_Sw_DataParams_t
Data structure for Random Number's Software layer implementation.
Definition: phCryptoRng.h:52
phCryptoRng_Seed
phStatus_t phCryptoRng_Seed(void *pDataParams, uint8_t *pSeed, uint8_t bSeedLength)
Seeds the random number generator with the given seed.
phbalReg_OpenPort
phStatus_t phbalReg_OpenPort(void *pDataParams)
Open communication port.
PHHAL_HW_SAMAV2_OPMODE_X_RC523
#define PHHAL_HW_SAMAV2_OPMODE_X_RC523
X-Mode operation (using Rc523).
Definition: phhalHw.h:259
phbalReg_PcscWin_Init
phStatus_t phbalReg_PcscWin_Init(phbalReg_PcscWin_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, uint8_t *pAtrBuffer, uint16_t wAtrBufSize)
Initialise the PCSC BAL component.
phhalHw_SamAV2_Cmd_SAM_AuthenticateHost
phStatus_t phhalHw_SamAV2_Cmd_SAM_AuthenticateHost(phhalHw_SamAV2_DataParams_t *pDataParams, uint8_t bAuthType_HostMode, uint16_t wRdKeyNo, uint16_t wRdKeyV, uint8_t bSamKeyNo, uint8_t bSamKeyV, uint8_t *pDivInput, uint8_t bDivInputLength)
Mutual 2-pass-AV1 or 3-pass-AV2 authentication between Host and SAM.
phhalHw_SamAV2_Init
phStatus_t phhalHw_SamAV2_Init(phhalHw_SamAV2_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, void *pBalDataParams, void *pReaderHalDataParams, void *pKeyStoreDataParams, void *pCryptoENCDataParams, void *pCryptoMACDataParams, void *pCryptoRngDataParams, uint8_t bOpMode, uint8_t bLogicalChannel, uint8_t *pTxBuffer, uint16_t wTxBufSize, uint8_t *pRxBuffer, uint16_t wRxBufSize)
Initialise the HAL component.
uint8_t
unsigned char uint8_t
8 bit unsigned integer
Definition: ph_TypeDefs.h:56
phhalHw_SamAV2_DataParams_t
SamAV2 HAL parameter structure.
Definition: phhalHw.h:293
phKeyStore_FormatKeyEntry
phStatus_t phKeyStore_FormatKeyEntry(void *pDataParams, uint16_t wKeyNo, uint16_t wNewKeyType)
Format a key entry to a new KeyType.