NXP Reader Library  v17.1.0.2535

Definitions for Key diversification programming mask. To be used with SAM_EncipherKeyEntry interface. More...

Collaboration diagram for EncipherKeyEntry:

Macros

#define PHHAL_HW_SAM_CMD_SAM_ENCIPHER_KEY_ENTRY_USE_DIVERSIFICATION   0x01U
 Option mask to include the diversification input in command frame.
 
#define PHHAL_HW_SAM_CMD_SAM_ENCIPHER_KEY_ENTRY_INCLUDE_SAMUID   0x02U
 Option mask to include the Sam UID in command frame.
 

Detailed Description

Definitions for Key diversification programming mask. To be used with SAM_EncipherKeyEntry interface.