NXP Reader Library  v17.1.0.2535

Sam Global macro Last Frame Indicator values that are used for most of the commands. More...

Collaboration diagram for Last Frame Indicator:

Macros

#define PHHAL_HW_SAM_ISO7816_LAST_FRAME   0x00U
 Indication last frame in a cipher sequence.
 
#define PHHAL_HW_SAM_ISO7816_CHAINED_FRAME   0xAFU
 Indication intermediate frame in a cipher sequence.
 

Detailed Description

Sam Global macro Last Frame Indicator values that are used for most of the commands.