NXP Reader Library  v17.1.0.2535

Definitions for indicating the interface call for first frame and add the required information to command buffer for exchange. For the next do not add the previously exchanged information. To be used with below mentioned interface(s) More...

Collaboration diagram for FirsFrame:

Macros

#define PHHAL_HW_SAM_CMD_PKI_FIRST_FRAME   0x80U
 Option mask for a framing the first frame of Decipher Data command.
 

Detailed Description

Definitions for indicating the interface call for first frame and add the required information to command buffer for exchange. For the next do not add the previously exchanged information. To be used with below mentioned interface(s)