Macro Definitions used across the whole SAM implementation. More...

Modules | |
| Reserved Length | |
| Macro Definitions used Transmit and Response buffer reserved length. | |
| Host Communication Mode | |
| Macro Definitions used for Host communication mode. | |
| Operation Mode | |
| Macro Definitions used for operation mode. To be used during Initialization of SAM component. | |
| Logical Channel | |
| Macro Definitions used for Logical Channel. To be used during Initialization of SAM component. | |
| Last Frame Indicator | |
| Sam Global macro Last Frame Indicator values that are used for most of the commands. | |
| SessionKey | |
| Sam Global macro Session Key values that are used for most of the commands. | |
| Configuration | |
| Macro Definitions for Get Config and Set Config interfaces. Refer Configuration under Generic HAL for all supported configuration identifiers. | |
Macro Definitions used across the whole SAM implementation.