NXP Reader Library  v17.1.0.2535

Macro Definitions for Get Config and Set Config interfaces. Refer Configuration under Generic HAL for all supported configuration identifiers. More...

Collaboration diagram for Configuration:

Macros

#define PHHAL_HW_SAM_CONFIG_HOSTMODE   (PH_CONFIG_CUSTOM_BEGIN + 0)
 Get / Set the HostMode; (e.g. More...
 
#define PHHAL_HW_SAM_CONFIG_DISABLE_NONX_CFG_MAPPING   (PH_CONFIG_CUSTOM_BEGIN + 1U)
 Disables the mapping of standard-configs to the Reader HAL if set to PH_ON; Default is PH_OFF; Only applicable in NonX-Mode.
 
#define PHHAL_HW_SAM_CONFIG_GET_SAM_ERROR_CODE   (PH_CONFIG_CUSTOM_BEGIN + 2U)
 Get the Actual Error Code returned by Sam.
 

Detailed Description

Macro Definitions for Get Config and Set Config interfaces. Refer Configuration under Generic HAL for all supported configuration identifiers.

Macro Definition Documentation

◆ PHHAL_HW_SAM_CONFIG_HOSTMODE

#define PHHAL_HW_SAM_CONFIG_HOSTMODE   (PH_CONFIG_CUSTOM_BEGIN + 0)

Get / Set the HostMode; (e.g.

AV4 ).