NXP Reader Library  v17.1.0.2535

Macro Definitions used for Logical Channel. To be used during Initialization of SAM component. More...

Collaboration diagram for Logical Channel:

Macros

#define PHHAL_HW_SAM_LOGICAL_CHANNEL_0   0x00
 Logical Channel zero.
 
#define PHHAL_HW_SAM_LOGICAL_CHANNEL_1   0x01U
 Logical Channel one.
 
#define PHHAL_HW_SAM_LOGICAL_CHANNEL_2   0x02U
 Logical Channel two.
 
#define PHHAL_HW_SAM_LOGICAL_CHANNEL_3   0x03U
 Logical Channel three.
 

Detailed Description

Macro Definitions used for Logical Channel. To be used during Initialization of SAM component.