Implementation of Utility interfaces.
More...
|
| phStatus_t | phhalHw_Sam_Utils_GetCheckLcLe (uint8_t *pCmd, uint16_t wCmdLen, uint8_t *pIsLcPresent, uint8_t *pLcLen, uint8_t *pIsLePresent) |
| | Get the length of LC and also check is LC and LE are present in the command frame. More...
|
| |
| phStatus_t | phhalHw_Sam_Utils_TruncateMacBuffer (uint8_t *pIoBuffer, uint8_t *pMacLen) |
| | Truncate a 16-Bytes MAC buffer into a 8-Bytes Buffer. More...
|
| |
| phStatus_t | phhalHw_Sam_Utils_GetLc (phhalHw_Sam_DataParams_t *pDataParams, uint8_t *pLC) |
| | Gets the current updated LC information. More...
|
| |
| phStatus_t | phhalHw_Sam_Utils_UpdateLc (phhalHw_Sam_DataParams_t *pDataParams) |
| | Update LC byte according to data already available in Buffer. More...
|
| |
| phStatus_t | phhalHw_Sam_Utils_UpdateP1 (phhalHw_Sam_DataParams_t *pDataParams, uint8_t p1) |
| | Update P1 byte according to data already available in Buffer. More...
|
| |
| phStatus_t | phhalHw_Sam_Utils_UpdateP2 (phhalHw_Sam_DataParams_t *pDataParams, uint8_t p2) |
| | Update P1byte according to data already available in Buffer. More...
|
| |
| phStatus_t | phhalHw_Sam_Utils_ResolveErrorCode (phhalHw_Sam_DataParams_t *pDataParams, uint8_t *pSw1Sw2) |
| | Parse Status Word Sw1Sw2 from the SAM and assign a equivalent custom code. More...
|
| |
| phStatus_t | phhalHw_Sam_Utils_GenerateHostAuthSessionKey (phhalHw_Sam_DataParams_t *pDataParams, uint8_t bKeyType, uint8_t *pRnd1, uint8_t *pRnd2, uint8_t *pSessionKey, uint8_t *pKeyLen) |
| | Session key generation for LockUnlock command. More...
|
| |
| phStatus_t | phhalHw_Sam_Utils_GenerateSessionKey (phhalHw_Sam_DataParams_t *pDataParams, uint8_t bKeyType, uint8_t *pRnd1, uint8_t *pRnd2, uint8_t *pSessionEncKey, uint8_t *pSessionMacKey, uint8_t *pKeyLen) |
| | Session key generation for AuthenticateHost command. More...
|
| |
| phStatus_t | phhalHw_Sam_Utils_GetSessionUploadKey (phhalHw_Sam_DataParams_t *pDataParams, uint8_t bMode, uint16_t wUploadCtr, uint8_t bKeyNo, uint8_t bKeyVer, uint8_t *pSessionKey, uint8_t *pKeyType) |
| | Session key generation for the command PLUpload. More...
|
| |
Implementation of Utility interfaces.
◆ phhalHw_Sam_Utils_GetCheckLcLe()
Get the length of LC and also check is LC and LE are present in the command frame.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pCmd | [In] Address of buffer that contains the command. |
| [in] | wCmdLen | [In] Length of the command. |
| [out] | pIsLcPresent | [Out] LC byte presence indicator. |
| [out] | pLcLen | [Out] Length of the payload of the command. |
| [out] | pIsLePresent | [Out] LE byte presence indicator. |
◆ phhalHw_Sam_Utils_TruncateMacBuffer()
Truncate a 16-Bytes MAC buffer into a 8-Bytes Buffer.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in,out] | pIoBuffer | [In, Out] The 16 bytes of computed MAC as input and 8 bytes of truncated MAC as output. |
| [in,out] | pMacLen | [In, Out] Non-Truncated MAC length as input and Truncated MAC length as output. |
◆ phhalHw_Sam_Utils_GetLc()
Gets the current updated LC information.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [out] | pLC | [Out] Provides the current updated LC information. |
◆ phhalHw_Sam_Utils_UpdateLc()
Update LC byte according to data already available in Buffer.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
◆ phhalHw_Sam_Utils_UpdateP1()
Update P1 byte according to data already available in Buffer.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | p1 | [In] Value for P1. |
◆ phhalHw_Sam_Utils_UpdateP2()
Update P1byte according to data already available in Buffer.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlaying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | p2 | [In] Value for P1. |
◆ phhalHw_Sam_Utils_ResolveErrorCode()
Parse Status Word Sw1Sw2 from the SAM and assign a equivalent custom code.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | pSw1Sw2 | [In] Pointer to the status code sent by the SAM. |
◆ phhalHw_Sam_Utils_GenerateHostAuthSessionKey()
Session key generation for LockUnlock command.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bKeyType | [In] The key type to be used (AES128 or AES192) |
| [in] | pRnd1 | [In] Pointer to Rnd1 data. |
| [in] | pRnd2 | [In] Pointer to Rnd2 data. |
| [out] | pSessionKey | [Out] The generated session key. |
| [out] | pKeyLen | [Out] Length of the Session key. |
◆ phhalHw_Sam_Utils_GenerateSessionKey()
Session key generation for AuthenticateHost command.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bKeyType | [In] The key type to be used (AES128 or AES192) |
| [in] | pRnd1 | [In] Pointer to Rnd1 data. |
| [in] | pRnd2 | [In] Pointer to Rnd2 data. |
| [out] | pSessionEncKey | [Out] The generate session encryption key. |
| [out] | pSessionMacKey | [Out] The generate session mac key. |
| [out] | pKeyLen | [Out] Length of the Session key. |
◆ phhalHw_Sam_Utils_GetSessionUploadKey()
Session key generation for the command PLUpload.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | bMode | [In] Mode to use for session key generation. Can be one of the below options.
- PHHAL_HW_CMD_SAM_SESSION_KEY_ENC "Session Encryption Key"
- PHHAL_HW_CMD_SAM_SESSION_KEY_MAC "Session MAC Key"
|
| [in] | wUploadCtr | [In] The upload counter value. |
| [in] | bKeyNo | [In] Key number using which the key will be taken from keystore for macing the session vectors. |
| [in] | bKeyVer | [In] Key version to be used. |
| [out] | pSessionKey | [Out] The generated session key. |
| [out] | pKeyType | [Out] The type of key used for session key generation. |