NXP Reader Library  v17.1.0.2535

These Components implement the additional ISO/IEC 14443-4 activation steps needed for ISO14443 Type-A cards. More...

Collaboration diagram for ISO/IEC14443-4A:

Modules

 Component : Software
 
 Component : Rd710
 end of group phpalI14443p4a_Sam_X
 
 Component : PCSC
 
 Component : SamAV2_X
 
 Component : SamAV3_X
 
 Component : Callback
 
 Component : Sam_X
 

Functions

phStatus_t phpalI14443p4a_Rats (void *pDataParams, uint8_t bFsdi, uint8_t bCid, uint8_t *pAts)
 Perform a ISO14443-4A "Request Answer to Select" command. More...
 
phStatus_t phpalI14443p4a_Pps (void *pDataParams, uint8_t bDri, uint8_t bDsi)
 Perform a ISO14443-4A "Protocol and Parameter Selection" command. More...
 
phStatus_t phpalI14443p4a_ActivateCard (void *pDataParams, uint8_t bFsdi, uint8_t bCid, uint8_t bDri, uint8_t bDsi, uint8_t *pAts)
 Perform ISO14443-4A Rats and Pps commands. More...
 
phStatus_t phpalI14443p4a_GetProtocolParams (void *pDataParams, uint8_t *pCidEnabled, uint8_t *pCid, uint8_t *pNadSupported, uint8_t *pFwi, uint8_t *pFsdi, uint8_t *pFsci)
 Retrieve the ISO14443-4A protocol parameters. More...
 

DRI/DSI Values

#define PHPAL_I14443P4A_DATARATE_106   0x00U
 DRI/DSI value for 106 kBit/s

 
#define PHPAL_I14443P4A_DATARATE_212   0x01U
 DRI/DSI value for 212 kBit/s

 
#define PHPAL_I14443P4A_DATARATE_424   0x02U
 DRI/DSI value for 424 kBit/s

 
#define PHPAL_I14443P4A_DATARATE_848   0x03U
 DRI/DSI value for 848 kBit/s

 

Detailed Description

These Components implement the additional ISO/IEC 14443-4 activation steps needed for ISO14443 Type-A cards.

Function Documentation

◆ phpalI14443p4a_Rats()

phStatus_t phpalI14443p4a_Rats ( void *  pDataParams,
uint8_t  bFsdi,
uint8_t  bCid,
uint8_t pAts 
)

Perform a ISO14443-4A "Request Answer to Select" command.

[FSDI to FSD conversion]
----------------------------------------------------------------------------------------
FSDI         | 00 | 01 | 02 | 03 | 04 | 05 | 06 | 07  | 08  | 09  | 0A   | 0B   | 0C   |
----------------------------------------------------------------------------------------
FSD (bytes)  | 16 | 24 | 32 | 40 | 48 | 64 | 96 | 128 | 256 | 512 | 1024 | 2018 | 4096 |
----------------------------------------------------------------------------------------
Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_PROTOCOL_ERRORInvalid response received.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bFsdi[In] Frame Size Integer; 0-8 (0xC for SW implementation to support 4k frames)
[in]bCid[In] Card Identifier; 0-14
[out]pAts[Out] Answer to Select; uint8_t[255]

◆ phpalI14443p4a_Pps()

phStatus_t phpalI14443p4a_Pps ( void *  pDataParams,
uint8_t  bDri,
uint8_t  bDsi 
)

Perform a ISO14443-4A "Protocol and Parameter Selection" command.

The following values for bDri and bDsi are possible:

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_PROTOCOL_ERRORInvalid response received.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bDri[In] Divisor Receive (PCD to PICC) Integer; 0-3
[in]bDsi[In] Divisor Send (PICC to PCD) Integer; 0-3

◆ phpalI14443p4a_ActivateCard()

phStatus_t phpalI14443p4a_ActivateCard ( void *  pDataParams,
uint8_t  bFsdi,
uint8_t  bCid,
uint8_t  bDri,
uint8_t  bDsi,
uint8_t pAts 
)

Perform ISO14443-4A Rats and Pps commands.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
PH_ERR_PROTOCOL_ERRORInvalid response received.
PH_ERR_FRAMING_ERRORBcc invalid.
OtherDepending on implementation and underlaying component.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]bFsdi[In] Frame Size Integer; 0-8 (0xC for SW implementation to support 4k frames)
[in]bCid[In] Card Identifier; 0-14
[in]bDri[In] Divisor Receive (PCD to PICC) Integer; 0-3
[in]bDsi[In] Divisor Send (PICC to PCD) Integer; 0-3
[out]pAts[Out] Answer to Select; uint8_t[255]

◆ phpalI14443p4a_GetProtocolParams()

phStatus_t phpalI14443p4a_GetProtocolParams ( void *  pDataParams,
uint8_t pCidEnabled,
uint8_t pCid,
uint8_t pNadSupported,
uint8_t pFwi,
uint8_t pFsdi,
uint8_t pFsci 
)

Retrieve the ISO14443-4A protocol parameters.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[out]pCidEnabled[Out] Unequal '0' if Card Identifier is enabled.
[out]pCid[Out] Card Identifier.
[out]pNadSupported[Out] Node Address Support; Unequal '0' if supported.
[out]pFwi[Out] Frame Waiting Integer.
[out]pFsdi[Out] PCD Frame Size Integer; 0-8 (0xC for SW implementation to support 4k frames).
[out]pFsci[Out] PICC Frame Size Integer; 0-8 (0xC for SW implementation to support 4k frames).