end of group phpalI14443p4a_Sam_X More...

Data Structures | |
| struct | phpalI14443p4a_Rd710_DataParams_t |
| ISO14443-4a parameter structure. More... | |
Macros | |
| #define | PHPAL_I14443P4A_RD710_ID 0x03 |
| ID for RD710 ISO14443-4A layer | |
Functions | |
| phStatus_t | phpalI14443p4a_Rd710_Init (phpalI14443p4a_Rd710_DataParams_t *pDataParams, uint16_t wSizeOfDataParams, phhalHw_Rd710_DataParams_t *pHalDataParams) |
| Initialise this layer. More... | |
end of group phpalI14443p4a_Sam_X
| phStatus_t phpalI14443p4a_Rd710_Init | ( | phpalI14443p4a_Rd710_DataParams_t * | pDataParams, |
| uint16_t | wSizeOfDataParams, | ||
| phhalHw_Rd710_DataParams_t * | pHalDataParams | ||
| ) |
Initialise this layer.
| PH_ERR_SUCCESS | Operation successful. |
| [in] | pDataParams | [In] Pointer to this layer's parameter structure |
| [in] | wSizeOfDataParams | [In] Specifies the size of the data parameter structure. |
| [in] | pHalDataParams | [In] Pointer to the parameter structure of the underlying layer |