Common commands that performs Activation of the VICC, Exchange to VICC, etc...
More...
|
| phStatus_t | phpalSli15693_ActivateCard (void *pDataParams, uint8_t bOption, uint8_t bFlags, uint8_t bAfi, uint8_t *pMask, uint8_t bMaskBitLen, uint8_t *pDsfid, uint8_t *pUid, uint8_t *pMoreCardsAvailable) |
| | Perform ISO15693 ActivateCard command. More...
|
| |
| phStatus_t | phpalSli15693_SendEof (void *pDataParams, uint8_t bOption, uint8_t *pDsfid, uint8_t *pUid, uint8_t *pUidLen, uint8_t *pData, uint16_t *pDataLen) |
| | Send a ISO15693 EOF (End of Frame). More...
|
| |
| phStatus_t | phpalSli15693_Exchange (void *pDataParams, uint16_t wOption, uint8_t *pTxBuffer, uint16_t wTxBuffLen, uint8_t **ppRxBuffer, uint16_t *pRxBuffLen) |
| | Perform ISO15693 Data Exchange with VICC. More...
|
| |
| phStatus_t | phpalSli15693_InProcessReplyASync (void *pDataParams, uint8_t *pTxBuffer, uint16_t wTxBuffLen, uint8_t *pResponse1, uint16_t *pResp1_Len, uint8_t *pResponse2, uint16_t *pResp2_Len) |
| | Perform ISO15693 Data Exchange with VICC with dual response for a single command. More...
|
| |
Common commands that performs Activation of the VICC, Exchange to VICC, etc...
◆ phpalSli15693_ActivateCard()
Perform ISO15693 ActivateCard command.
- This function activates the first VICC detected during the collision resolution and optionally move it to selected state based on the wOption specified.
- bOption can be one of:
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | bOption | [In] Selected or addressed. Refer description for supported options. |
| [in] | bFlags | [In] Request flags byte. Refer below set of flags
|
| [in] | bAfi | [In] Application Family Identifier. |
| [in] | pMask | [In] UID mask, holding known UID bits. |
| [in] | bMaskBitLen | [In] Number of UID bits within pMask. |
| [out] | pDsfid | [Out] Data Storage Format Identifier. |
| [out] | pUid | [Out] Received UID of first found card |
| [out] | pMoreCardsAvailable | [Out] If there are more cards available this value is different from zero. |
◆ phpalSli15693_SendEof()
Send a ISO15693 EOF (End of Frame).
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | bOption | [In] Option parameter. Refer description for supported options. |
| [out] | pDsfid | [Out] Data Storage Format Identifier. |
| [out] | pUid | [Out] Received UID |
| [out] | pUidLen | [Out] Length of bytes available in pUid buffer. |
| [out] | pData | [Out] Received data. |
| [out] | pDataLen | [Out] Length of bytes available in pData buffer. |
◆ phpalSli15693_Exchange()
Perform ISO15693 Data Exchange with VICC.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | wOption | [In] Buffering options. Refer description for supported options. |
| [in] | pTxBuffer | [In] Data to be transmitted to VICC. |
- Note
- : Flags, IC MFC code and UID will be added automatically by the library internally.
- Parameters
-
| [in] | wTxBuffLen | [In] Length of bytes available in pTxBuffer buffer. |
| [out] | ppRxBuffer | [Out] Received information from VICC. |
| [out] | pRxBuffLen | [Out] Length of bytes available in ppRxBuffer buffer. |
◆ phpalSli15693_InProcessReplyASync()
Perform ISO15693 Data Exchange with VICC with dual response for a single command.
- Note
- :
- The implementation is based on ISO/IEC 15693-3:2019, VICC in-reply process — Asynchronous mode, section 9.8.3.3
- The response is given out as is received from the VICC removing the Flags in case of SUCCESS or FAILURE.
- The actual error code received from VICC can be retrieved using SetConfig with Additional Information as configuration identifier.
- Validation of the response is not carried out by this interface.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | pTxBuffer | [In] Data to be transmitted to VICC. |
- Note
- : Flags, IC MFC code and UID will be added automatically by the library internally.
- Parameters
-
| [in] | wTxBuffLen | [In] Length of bytes available in pTxBuffer buffer. |
| [out] | pResponse1 | [Out] First Information received from VICC. |
| [out] | pResp1_Len | [Out] Length of bytes available in pResponse1 buffer. |
| [out] | pResponse2 | [Out] Second Information received from VICC. |
| [out] | pResp2_Len | [Out] Length of bytes available in pResponse2 buffer. |