NXP Reader Library
v17.1.0.2535
Data Fields
phKeyStore_Rc663_DataParams_t Struct Reference
Common
»
KeyStore
»
Component : Rc663
Rc663 parameter structure.
More...
Data Fields
uint16_t
wId
Layer ID for this component, NEVER MODIFY!
void *
pHalDataParams
Pointer to the parameter structure of the underlying layer.
Detailed Description
Rc663 parameter structure.
The documentation for this struct was generated from the following file:
phKeyStore.h
phKeyStore_Rc663_DataParams_t
Generated on Sun Aug 31 2025 16:20:43 for NXP Reader Library by © NXP 2021