NXP Reader Library  v17.1.0.2535
phKeyStore_Sam_DataParams_t Struct Reference

SAM (AV4 and future SAM's) parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_Sam_DataParams_tpHalDataParams
 Pointer to the parameter structure of the underlying layer.
 
uint8_t aSet [2U]
 Configuration settings.
 
uint8_t aExtSet [2U]
 Extended configuration settings.
 
uint8_t aDFAid [3U]
 DESFire application ID.
 
uint8_t bDFKeyNo
 DESFire key number.
 
uint8_t bKeyNoCEK
 Key Number of Change Entry Key.
 
uint8_t bKeyVCEK
 Key Version of Change Entry Key.
 
uint8_t bRefNoKUC
 Reference number of key usage counter.
 
uint8_t bKeyNoAEK
 Key Number of Access Entry Key.
 
uint8_t bKeyVAEK
 Key Version of Access Entry Key.
 
uint8_t bKeyNoCKUC
 Key Number of Change KUC.
 
uint8_t bKeyVCKUC
 Key Version of Change KUC.
 
uint8_t b2K3DESOption
 Option for single DES and 2 Key Triple DES keys. More...
 
uint8_t bIsLRPKey
 Option for LRP key type. More...
 

Detailed Description

SAM (AV4 and future SAM's) parameter structure.

Field Documentation

◆ b2K3DESOption

uint8_t phKeyStore_Sam_DataParams_t::b2K3DESOption

Option for single DES and 2 Key Triple DES keys.

Can be set either to

◆ bIsLRPKey

uint8_t phKeyStore_Sam_DataParams_t::bIsLRPKey

Option for LRP key type.

If set indicated that the AES key is of LRP type.


The documentation for this struct was generated from the following file: