NXP Reader Library  v17.1.0.2535
phpalMifare_Sam_X_DataParams_t Struct Reference

SAM (AV4 and future SAM's) PAL-MIFARE parameter structure. More...

Data Fields

uint16_t wId
 Layer ID for this component, NEVER MODIFY!
 
phhalHw_Sam_DataParams_tpHalDataParams
 Pointer to the parameter structure of the underlying HAL layer.
 
void * pPalI14443p4DataParams
 Pointer to the parameter structure of the underlying ISO14443-4 layer.
 

Detailed Description

SAM (AV4 and future SAM's) PAL-MIFARE parameter structure.


The documentation for this struct was generated from the following file: