NXP Reader Library  v17.1.0.2535
Deprecated List
Global phalICode_AuthenticateTAM1 (void *pDataParams, uint8_t bOption, uint8_t bKeyNo, uint8_t bKeyVer, uint8_t bKeyNoCard, uint8_t *pDivInput, uint8_t bDivLen)
Refer TAM Authentication
Global phalICode_AuthenticateTAM2 (void *pDataParams, uint8_t bOption, uint8_t bKeyNo, uint8_t bKeyVer, uint8_t bKeyNoCard, uint8_t *pDivInput, uint8_t bDivLen, uint8_t bBlockSize, uint8_t bBlockCount, uint8_t bProfile, uint8_t bProtMode, uint16_t wOffset, uint8_t *pCustomData, uint16_t *pCustomDataLen)
Refer TAM Authentication
Module phbalReg_Rd710Sam
RD710SAM component is obsolete and will be removed.