NXP Reader Library  v17.1.0.2535
Component : Software

Software implementation. More...

Collaboration diagram for Component : Software:

Data Structures

struct  phCidManager_Sw_DataParams_t
 Cid Manager parameter structure. More...
 

Macros

#define PH_CIDMANAGER_SW_ID   0x01U
 ID for Software component.
 

Functions

phStatus_t phCidManager_Sw_Init (phCidManager_Sw_DataParams_t *pDataParams, uint16_t wSizeOfDataParams)
 Initialise this layer. More...
 

Detailed Description

Software implementation.

Function Documentation

◆ phCidManager_Sw_Init()

phStatus_t phCidManager_Sw_Init ( phCidManager_Sw_DataParams_t pDataParams,
uint16_t  wSizeOfDataParams 
)

Initialise this layer.

Returns
Status code
Return values
PH_ERR_SUCCESSOperation successful.
Parameters
[in]pDataParams[In] Pointer to this layer's parameter structure.
[in]wSizeOfDataParams[In] Specifies the size of the data parameter structure.