Supported Hashing algorithms. Also known as Message Digest (MD). More...

Macros | |
| #define | PH_CRYPTOASYM_HASH_ALGO_NOT_APPLICABLE 0U |
| None. More... | |
| #define | PH_CRYPTOASYM_HASH_ALGO_SHA224 3U |
| The SHA-224 hashing algorithm. | |
| #define | PH_CRYPTOASYM_HASH_ALGO_SHA256 4U |
| The SHA-256 hashing algorithm. | |
| #define | PH_CRYPTOASYM_HASH_ALGO_SHA384 5U |
| The SHA-384 hashing algorithm. | |
| #define | PH_CRYPTOASYM_HASH_ALGO_SHA512 6U |
| The SHA-512 hashing algorithm. | |
Supported Hashing algorithms. Also known as Message Digest (MD).
| #define PH_CRYPTOASYM_HASH_ALGO_NOT_APPLICABLE 0U |
None.
Hashing will not be performed for the message.