NXP Reader Library  v17.1.0.2535
Examples

ASymmetric Crypto Examples. More...

Collaboration diagram for Examples:

Modules

 01_GenerateKeyPair
 Example code to Generate a Key Pair.
 
 02_LoadKey
 Example code to load Private or Public Keys from Keystore.
 
 03_LoadKeyDirect
 Example code to load Private or Public keys directly to this component.
 
 04_ExportKey
 Example code to export Private or Public Keys from Keystore.
 
 05_Signature
 Example code to Generate Signature for the raw input message.
 
 06_Verification
 Example code to verify the raw message and signature.
 
 07_ECDH
 Example code to Compute Shared secret between both the parties.
 

Detailed Description

ASymmetric Crypto Examples.