Internal Functions of the Symmetric Cryptography component.
More...
|
| phStatus_t | phCryptoSym_Sw_EncryptBlock (phCryptoSym_Sw_DataParams_t *pDataParams, uint8_t PH_CRYTOSYM_SW_FAST_RAM *pBlock) |
| | Generic interface function for encryption of a single AES/DES data block. More...
|
| |
| phStatus_t | phCryptoSym_Sw_DecryptBlock (phCryptoSym_Sw_DataParams_t *pDataParams, uint8_t PH_CRYTOSYM_SW_FAST_RAM *pBlock) |
| | Generic interface function for decryption of a single AES/DES data block. More...
|
| |
| void | phCryptoSym_Sw_CMAC_LeftShift (const uint8_t *pInBuffer, uint8_t bInputLen, uint8_t *pOutBuffer) |
| | Implements the left shift according to CMAC standard. More...
|
| |
| phStatus_t | phCryptoSym_Sw_CMAC_GenerateK1K2 (phCryptoSym_Sw_DataParams_t *pDataParams, uint8_t *pSubKey1, uint8_t *pSubKey2) |
| | Implements sub key generation according to CMAC standard. More...
|
| |
| phStatus_t | phCryptoSym_Sw_Diversify_CMAC (phCryptoSym_Sw_DataParams_t *pDataParams, const uint8_t *pData, uint16_t wDataLength, uint8_t *pMac, uint8_t *pMacLength) |
| | Calculate CMAC for Key diversification. More...
|
| |
Internal Functions of the Symmetric Cryptography component.
◆ phCryptoSym_Sw_EncryptBlock()
Generic interface function for encryption of a single AES/DES data block.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in,out] | pBlock | [InOut] IO buffer for the data block to perform the encryption on. |
◆ phCryptoSym_Sw_DecryptBlock()
Generic interface function for decryption of a single AES/DES data block.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in,out] | pBlock | [InOut] IO buffer for the data block to perform the decryption on. |
◆ phCryptoSym_Sw_CMAC_LeftShift()
| void phCryptoSym_Sw_CMAC_LeftShift |
( |
const uint8_t * |
pInBuffer, |
|
|
uint8_t |
bInputLen, |
|
|
uint8_t * |
pOutBuffer |
|
) |
| |
Implements the left shift according to CMAC standard.
- Parameters
-
| [in] | pInBuffer | [In] Array containing the input buffer to be shifted. |
| [in] | bInputLen | [In] Length of the input buffer. |
| [out] | pOutBuffer | [Out] Array containing the output buffer where the shifted value is stored. |
◆ phCryptoSym_Sw_CMAC_GenerateK1K2()
Implements sub key generation according to CMAC standard.
Implementation according to SUBK(K) section 6 of NIST SP_800-38B
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [out] | pSubKey1 | [Out] Destination pointer for CMAC subkey 1 |
| [out] | pSubKey2 | [Out] Destination pointer for CMAC subkey 2 |
◆ phCryptoSym_Sw_Diversify_CMAC()
Calculate CMAC for Key diversification.
- Returns
- Status code
- Return values
-
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layers parameter structure. |
| [in] | pData | [In] Input data; uint8_t[wDataLength]. |
| [in] | wDataLength | [In] Number of input data bytes. |
| [out] | pMac | [Out] Output MAC block; uint8_t[16]. |
| [out] | pMacLength | [Out] Length of MAC. |