Interfaces for ASymmetric keys of KeyStore component.
More...
|
| phStatus_t | phKeyStore_SetKeyASym (void *pDataParams, uint16_t wKeyNo, uint16_t wPos, uint16_t wKeyType, uint16_t wKeyInfo, uint8_t *pKey, uint16_t wKeyLen) |
| | Change a Asymmetric Private or Public key entry in Un-compressed Binary format. More...
|
| |
| phStatus_t | phKeyStore_GetKeyASym (void *pDataParams, uint16_t wKeyNo, uint16_t wPos, uint16_t wKeyPairType, uint16_t *pKeyType, uint8_t *pCurveID, uint8_t *pKey, uint16_t *pKeyLen) |
| | Get a asymmetric key. More...
|
| |
| phStatus_t | phKeyStore_GetCurveID (void *pDataParams, uint16_t wKeyNo, uint16_t wPos, uint8_t *pCurveID) |
| | Get a asymmetric key ECC Curve ID. More...
|
| |
Interfaces for ASymmetric keys of KeyStore component.
◆ phKeyStore_SetKeyASym()
Change a Asymmetric Private or Public key entry in Un-compressed Binary format.
- Note
- This interface should be called more than ones to load Private or Public Key.
- One Key number at a specific position can hold both Private and Public Key.
- Public Key alone can be stored also.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wKeyNo | [In] Key number of the KeyStore to be loaded. |
| [in] | wPos | [In] Position at which the Key should be updated.
- Should be the Key position to set the key to DataParams pKeyEntries member.
|
| [in] | wKeyType | [In] New Key type of the KeyEntry (predefined type of KeyType).
|
| [in] | wKeyInfo | [In] Type of Key pair and Curve to save.
- Refer Key Pair to save.
- Refer CurveID for type of Curve available in pKey buffer.
|
| [in] | pKey | [In] Pointer to the key itself.
- Private Key should be equal to the provided CurveID in wKeyInfo parameter.
- Public Key should be twice the length of Private Key including the Uncompressed notation at beginning of the buffer.
|
| [in] | wKeyLen | [In] Length of bytes available in pKey buffer. |
◆ phKeyStore_GetKeyASym()
Get a asymmetric key.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wKeyNo | [In] Key number of the KeyStore to be retrieved. |
| [in] | wPos | [In] Position at which the Key should be retrieved.
- Should be the Key position to get the key from DataParams pKeyEntries member.
|
| [in] | wKeyPairType | [In] Type of Key-pair to be retrieved.
|
| [in] | pKeyType | [In] Type of key being saved earlier.
|
| [in] | pCurveID | [In] One of the Curve ID's. |
| [out] | pKey | [Out] Pointer to the key itself. The buffer size should be equal or greater than the Size of the stored key. |
| [out] | pKeyLen | [Out] Length of bytes available in pKey buffer. |
◆ phKeyStore_GetCurveID()
Get a asymmetric key ECC Curve ID.
- Returns
- Status code
- Return values
-
| PH_ERR_SUCCESS | Operation successful. |
| Other | Depending on implementation and underlying component. |
- Parameters
-
| [in] | pDataParams | [In] Pointer to this layer's parameter structure. |
| [in] | wKeyNo | [In] Key number of the KeyStore to be retrieved. |
| [in] | wPos | [In] Position at which the Key should be retrieved.
- Should be the Key position to get the key from DataParams pKeyEntries member.
|
| [out] | pCurveID | [Out] Provided the CurveID of the provided Key informations. Will return one of the following mentioned in Curve ID's |