NXP Reader Library  v17.1.0.2535
Type Definitions

Contains definitions for types defined within NxpRdLib. More...

Collaboration diagram for Type Definitions:

Unsigned Types

typedef unsigned char uint8_t
 8 bit unsigned integer
 
typedef unsigned short uint16_t
 16 bit unsigned integer
 
typedef unsigned int uint32_t
 32 bit unsigned integer
 
typedef unsigned long uint64_t
 64 bit unsigned integer
 
#define __uint8_t_defined
 
#define __uint16_t_defined
 
#define __uint32_t_defined
 
#define __uint64_t_defined
 

Signed Types

typedef signed char int8_t
 8 bit signed integer
 
typedef short int16_t
 16 bit signed integer
 
typedef int int32_t
 32 bit signed integer
 
typedef long int64_t
 64 bit signed integer
 
#define __int8_t_defined
 
#define __int16_t_defined
 
#define __int32_t_defined
 
#define __int64_t_defined
 

Floating-Point Types

typedef float float32_t
 32 bit floating point
 
#define __float32_t_defined
 

Double-Precision Floating Point Types

typedef double float64_t
 64 bit floating point
 
#define __float64_t_defined
 

Boolean Types

#define __BOOL_DEFINED
 
#define bool   unsigned char;
 
#define true   1
 
#define false   0
 

Other Types

typedef uint16_t phStatus_t
 phcsBfl_Status_t is a signed short value, using the positive range. More...
 
#define NULL   0
 

Detailed Description

Contains definitions for types defined within NxpRdLib.

Typedef Documentation

◆ phStatus_t

phcsBfl_Status_t is a signed short value, using the positive range.

High byte: Category (group) Identifier.
Low byte : Error Specifier.